This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-J721E:TI-tisdk-firmwarebb:do_fetch 问题

Guru**** 2541730 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1193350/processor-sdk-j721e-ti-tisdk-firmware-bb-do_fetch-problems

器件型号:PROCESSOR-SDK-J721E

我正在尝试使用以下命令行构建默认映像:

toolchain_base=/home machine=j7-evm bitbake -k tisdk-default-image

输出:

ERROR: ti-tisdk-firmware-1.0-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'repo://git.ti.com/processor-sdk/psdk_repo_manifests.git;protocol=git;branch=refs/tags/REL.PSDK.JACINTO.08.05.00.08a;manifest=vision_apps_yocto.xml')
ERROR: Logfile of failure stored in: /home/ti-processor-sdk-linux-j7-evm-08_05_00_08/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/ti-tisdk-firmware/1.0-r0/temp/log.do_fetch.499285
ERROR: Task (/home/ti-processor-sdk-linux-j7-evm-08_05_00_08/yocto-build/sources/meta-psdkla/recipes-tisdk/ti-tisdk-firmware/ti-tisdk-firmware.bb:do_fetch) failed with exit code '1'

Proxys 都是为其他提取物/配方设置和工作的、但这是唯一使用 REPO 的配方://

是否需要做些什么才能使 REPO://协议正常工作?

请任何人提出建议。

/Bo