尊敬的 TI 专家
您能否向我提供 Windows 或 Ubuntu 版本的 SK-AM62A-LP DCC 调优工具?
我已经准备好调试 ISP、但缺少工具
我在 e2e 中搜索 DCC 车削工具、找到以下链接并请求
TDA4VM:TDA4VM ISP DCC 调优工具-处理器论坛-处理器- TI E2E 支持论坛
请求链接
但什么也没得到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 TI 专家
您能否向我提供 Windows 或 Ubuntu 版本的 SK-AM62A-LP DCC 调优工具?
我已经准备好调试 ISP、但缺少工具
我在 e2e 中搜索 DCC 车削工具、找到以下链接并请求
TDA4VM:TDA4VM ISP DCC 调优工具-处理器论坛-处理器- TI E2E 支持论坛
请求链接
但什么也没得到
好的。 我有现成的工具、但没有从目标(am62ax-LP-EVM 板)获取原始数据
PROCESSOR-SDK-AM68A:[AM68A]如何通过 TI EVK 和 DCC 工具捕获原始图像-传感器论坛-传感器- TI E2E 支持论坛
我的 SDK 版本是 sdk806.wic.xz
1. Navigate to /opt/edgeai-tiovx-modules/ 2. In the CMakeLists.txt file, modify (ENABLE_DCC_TOOL "Enable DCC Tuning Tool Support" OFF -> ON) 3. mkdir build 4. cd build 5. cmake .. 6. make -j2 7. make install
重新启动计算机并打开 imx219摄像头
systemctl stop weston.service media-ctl -V '"imx219 4-0010":0 [fmt:SRGGB10_1X10/1920x1080 field:none]' gst-launch-1.0 v4l2src device=/dev/video2 io-mode=dmabuf-import ! \ video/x-bayer, width=1920, height=1080, framerate=30/1, format=rggb10 ! \ tiovxisp sink_0::device=/dev/v4l-subdev2 \ sensor-name="SENSOR_SONY_IMX219_RPI" \ dcc-isp-file=/opt/imaging/imx219/dcc_viss_10b.bin \ sink_0::dcc-2a-file=/opt/imaging/imx219/dcc_2a_10b.bin format-msb=9 ! \ video/x-raw, format=NV12, width=1920, height=1080, framerate=30/1 ! \ kmssink driver-name=tidss sync=false


以太网网络链路 RJ45直接连接到 PC、
可以相互 ping 通的机器的输入 IP



然后单击 SAVE RAW 或 YUV FORM CAMERA、然后工具会打印
捕获原始图像时出错

我们有一个捕获操作位于
gst-launch-1.0 v4l2src device=/dev/video2 io-mode=dmabuf-import ! \ video/x-bayer, width=1920, height=1080, framerate=30/1, format=rggb10 ! \ tiovxisp sink_0::device=/dev/v4l-subdev2 \ sensor-name="SENSOR_SONY_IMX219_RPI" \ dcc-isp-file=/opt/imaging/imx219/dcc_viss_10b.bin \ sink_0::dcc-2a-file=/opt/imaging/imx219/dcc_2a_10b.bin format-msb=9 ! \ video/x-raw, format=NV12, width=1920, height=1080, framerate=30/1 ! \ kmssink driver-name=tidss sync=false
尊敬的大维:
我的 SDK 版本是 sdk806.wic.xz
您是否在使用 SDK 8.6? 实时调优在8.6版上不起作用。 您能否改用最新版本(9.1)?
此致、
建中市
我下载图像从链接,但我发现这个版本有问题摄像头不能工作,我把 dtb releasivative img ,它不能工作
https://www.ti.com.cn/tool/cn/download/PROCESSOR-SDK-LINUX - AM62A/09.01.00.07

BOOT/uEnv.txt # This uEnv.txt file can contain additional environment settings that you # want to set in U-Boot at boot time. This can be simple variables such # as the serverip or custom variables. The format of this file is: # variable=value # NOTE: This file will be evaluated after the bootcmd is run and the # bootcmd must be set to load this file if it exists (this is the # default on all newer U-Boot images. This also means that some # variables such as bootdelay cannot be changed by this file since # it is not evaluated until the bootcmd is run. # Setting the right U-Boot environment variables name_overlays=
uEnv.txt
psdk_setup_file=.psdk_setup
check_psdk_setup=load mmc 1:1 ${loadaddr} ${psdk_setup_file}
# Reset to the default environment
do_psdk_setup=env default -f -a; saveenv
# If not previously configured, then configure the environment and indicate this by writing a file
uenvcmd=if run check_psdk_setup; then echo "Already setup."; else run do_psdk_setup; mw.b ${loadaddr} 0 1; fatwrite mmc 1:1 ${loadaddr} .psdk_setup 1; reset; fi
dorprocboot=0
name_overlays=k3-am62a7-sk-csi2-imx219.dtbo
我替换从 sdk806复制的 uEvent.txt ,它也 dmesg|grep imx219没有
Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => => => => => => => => printenv name_overlays ## Error: "name_overlays" not defined
=> setenv name_overlays k3-am62a7-sk-csi2-imx219.dtbo => printenv name_overlays name_overlays=k3-am62a7-sk-csi2-imx219.dtbo =>
我在 u-boot 上设置 env ,并发送 boot cmd ,它仍然没有关于 imx219的信息
=> printenv name_overlays ## Error: "name_overlays" not defined => savee Unknown command 'savee' - try 'help' => setenv name_overlays k3-am62a7-sk-csi2-imx219.dtbo => boot switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 487 bytes read in 21 ms (22.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 22 ms (0 Bytes/s) Already setup. ## Error: "main_cpsw0_qsgmii_phyinit" not defined 20302336 bytes read in 828 ms (23.4 MiB/s) 57364 bytes read in 26 ms (2.1 MiB/s) Working FDT set to 88000000 Failed to load '/boot/dtb/ti/k3-am62a7-sk-csi2-imx219.dtbo' ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK Working FDT set to 8feee000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
尊敬的大维:
dtbo 文件名在9.1中被更改:
root@am62axx-evm:~# ls /boot/dtb/ti/k3-am62x-sk-csi2-imx219.dtbo /boot/dtb/ti/k3-am62x-sk-csi2-imx219.dtbo
应使用"setenv name_overlays k3-am62x-sk-csi2-imx219.dtbo"。
此致、
建中市
尊敬的 Daiwi:
我已 使用 SDK 9.1验证了 IMX219。 如果您只需在 /run/media/BOOT-mmcblk1p1/uEnv.txt 中添加以下内容、它应该可以正常工作、并且您不需要从 u-boot 设置 env:
name_overlays=k3-am62x-sk-csi2-imx219.dtbo
您能否查看 dmesg 并了解 dtbo 是否正确加载? 如果你不介意、可以在这里分享 dmesg 吗?
谢谢你。
建中市
是的,它可以打开相机
cd edgeai-tiovx-模块/
LS
VI CMakeLists.txt
option(INSTALL_SRC "Install src under /opt" OFF) option(ENABLE_DCC_TOOL "Enable DCC Tuning Tool Support" ON)
mkdir 构建
CD 编译/
Cmake ../
生成-j
进行安装
历史
同步
重新启动
检查网络

打开 DCC 工具



失败
systemctl disable weston systemctl disable edgeai-init systemctl stop edgeai-init v4l2-ctl --list-devices media-ctl -V '"imx219 4-0010":0 [fmt:SRGGB10_1X10/1920x1080 field:none]' gst-launch-1.0 -v v4l2src device=/dev/video3 io-mode=dmabuf-import ! \ video/x-bayer, width=1920, height=1080, framerate=30/1, format=rggb10 ! \ tiovxisp sink_0::device=/dev/v4l-subdev2 sensor-name="SENSOR_SONY_IMX219_RPI" \ dcc-isp-file=/opt/imaging/imx219/linear/dcc_viss_10b.bin sink_0::dcc-2a-file=/opt/imaging/imx219/linear/dcc_2a_10b.bin format-msb=9 ! \ video/x-raw, format=NV12, width=1920, height=1080, framerate=30/1 ! kmssink driver-name=tidss

我尝试它,它可以从 DCC 工具捕获,为什么 sdk806不捕获,
更年期/opt/edgeai-tiovx-modules ?
很高兴它最终为您效劳。
为什么 sdk806不捕获,
更年期/opt/edgeai-tiovx-modules ?
[/报价]是的、在 SDK 8.6上启用实时调优时、tiovx-modules 没有构建。
此致、
建中市