主题中讨论的其他器件:TFP410、 TLV320AIC26
运行"bitbake --继续 tisdk-edgeai-image",我不断收到以下错误。 我已验证我的构建机器上安装了 repo。
WARNING: ti-vision-apps-1.0-r0_edgeai_0 do_fetch: Failed to fetch URL repo://git.ti.com/processor-sdk/psdk_repo_manifests.git;protocol=git;branch=refs/tags/REL.PSDK.ANALYTICS.09.00.00.01;manifest=vision_apps_yocto.xml, attempting MIRRORS if available
ERROR: ti-vision-apps-1.0-r0_edgeai_0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export PATH="/work/sources/oe-core/scripts:/work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/recipe-sysroot-native/usr/bin/aarch64-oe-linux:/work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/recipe-sysroot/usr/bin/crossscripts:/work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/recipe-sysroot-native/usr/sbin:/work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/recipe-sysroot-native/usr/bin:/work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/recipe-sysroot-native/sbin:/work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/recipe-sysroot-native/bin:/work/sources/bitbake/bin:/work/build/arago-tmp-default-glibc/hosttools"; export HOME="/home/pokyuser"; /usr/bin/env repo sync failed with exit code 1, output:
error: command 'sync' requires repo to be installed first.
Use "repo init" to install it here.
ERROR: ti-vision-apps-1.0-r0_edgeai_0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'repo://git.ti.com/processor-sdk/psdk_repo_manifests.git;protocol=git;branch=refs/tags/REL.PSDK.ANALYTICS.09.00.00.01;manifest=vision_apps_yocto.xml')
ERROR: Logfile of failure stored in: /work/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ti-vision-apps/1.0-r0_edgeai_0/temp/log.do_fetch.1131
ERROR: Task (/work/sources/meta-edgeai/recipes-tisdk/ti-psdk-rtos/ti-vision-apps.bb:do_fetch) failed with exit code '1'