主题中讨论的其他器件:SK-AM62、 AM62A7、
你好
我们目前正在使用 SDK 9.01并应用 Falcon 模式。
要从 eMMC 引导、我将引导参数设置为如下所示。
bootargs = "console=ttyS2,115200 root=/dev/mmcblk0p1 rw rootfstype=ext4";
但是、引导后、内核模块加载失败。
日志如下所示。 是否有解决方案?
root@am62axx-evm:/opt/edgeai-gst-apps# systemctl status systemd-modules-load.service
x systemd-modules-load.service - Load Kernel Modules
Loaded: loaded (/lib/systemd/system/systemd-modules-load.service; static)
Active: failed (Result: exit-code) since Thu 2022-04-28 18:20:43 UTC; 29s ago
Docs: man:systemd-modules-load.service(8)
man:modules-load.d(5)
Process: 171 ExecStart=/lib/systemd/systemd-modules-load (code=exited, status=1/FAILURE)
Main PID: 171 (code=exited, status=1/FAILURE)
Apr 28 18:20:43 am62axx-evm systemd-modules-load[171]: Failed to insert module 'cryptodev': Cannot allocate memory
Apr 28 18:20:43 am62axx-evm systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE
Apr 28 18:20:43 am62axx-evm systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
Apr 28 18:20:43 am62axx-evm systemd[1]: Failed to start Load Kernel Modules.
Notice: journal has been rotated since unit was started, output may be incomplete.