This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-J722S:运行 onnx 编译失败

Guru**** 2543840 points
Other Parts Discussed in Thread: AM67A

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1435070/processor-sdk-j722s-run-onnx-compilation-fail

器件型号:PROCESSOR-SDK-J722S
主题中讨论的其他器件:AM67A

工具与软件:

嗨、团队:

我尝试通过 https://github.com/TexasInstruments/edgeai-tidl-tools/blob/master/examples/jupyter_notebooks/custom-model-onnx.ipynb 运行示例代码来转换模型

但我收到以下错误:

*************** EP Error ***************
EP Error Unknown Provider Type: TIDLCompilationProvider when using ['TIDLCompilationProvider', 'CPUExecutionProvider']
Falling back to ['CPUExecutionProvider'] and retrying.
****************************************

检查是否设置了 TIDL_TOOLS_PATH、并确保路径具有"tidl_model_import_onnx.SO"

请帮助我修复此症状

感谢您的帮助。

[备份]

下面的代码:

import os
import tqdm
import cv2
import numpy as np
import onnxruntime as rt
import shutil
from scripts.utils import imagenet_class_to_name, download_model
import matplotlib.pyplot as plt
from pathlib import Path
from IPython.display import Markdown as md
from scripts.utils import loggerWritter
from scripts.utils import get_svg_path
import onnx

def preprocess(image_path):
    
    # read the image using openCV
    img = cv2.imread(image_path)
    
    # convert to RGB
    img = img[:,:,::-1]
    
    # Most of the onnx models are trained using
    # 224x224 images. The general rule of thumb
    # is to scale the input image while preserving
    # the original aspect ratio so that the
    # short edge is 256 pixels, and then
    # center-crop the scaled image to 224x224
    orig_height, orig_width, _ = img.shape
    short_edge = min(img.shape[:2])
    new_height = (orig_height * 256) // short_edge
    new_width = (orig_width * 256) // short_edge
    img = cv2.resize(img, (new_width, new_height), interpolation=cv2.INTER_CUBIC)

    startx = new_width//2 - (224//2)
    starty = new_height//2 - (224//2)
    img = img[starty:starty+224,startx:startx+224]
    
    # apply scaling and mean subtraction.
    # if your model is built with an input
    # normalization layer, then you might
    # need to skip this
    img = img.astype('float32')
    for mean, scale, ch in zip([128, 128, 128], [0.0078125, 0.0078125, 0.0078125], range(img.shape[2])):
            img[:,:,ch] = ((img.astype('float32')[:,:,ch] - mean) * scale)
    img = np.expand_dims(img,axis=0)
    img = np.transpose(img, (0, 3, 1, 2))
    
    return img
calib_images = [
'sample-images/elephant.bmp',
'sample-images/bus.bmp',
'sample-images/bicycle.bmp',
'sample-images/zebra.bmp',
]
output_dir = 'custom-artifacts/onnx/resnet18_opset9.onnx'
onnx_model_path = 'models/public/onnx/resnet18_opset9.onnx'
download_model(onnx_model_path)
onnx.shape_inference.infer_shapes_path(onnx_model_path, onnx_model_path)
#compilation options - knobs to tweak 
num_bits =8
accuracy =1

log_dir = Path("logs").mkdir(parents=True, exist_ok=True)

# stdout and stderr saved to a *.log file.  
with loggerWritter("logs/custon-model-onnx"):

# model compilation options
    compile_options = {
        'tidl_tools_path' : os.environ['TIDL_TOOLS_PATH'],
        'artifacts_folder' : output_dir,
        'tensor_bits' : num_bits,
        'accuracy_level' : accuracy,
        'advanced_options:calibration_frames' : len(calib_images), 
        'advanced_options:calibration_iterations' : 3, # used if accuracy_level = 1
        'advanced_options:add_data_convert_ops' : 1,
        'debug_level' : 1,
        #'deny_list' : "MaxPool" #Comma separated string of operator types as defined by ONNX runtime, ex "MaxPool, Concat"
    }
# create the output dir if not present
# clear the directory
os.makedirs(output_dir, exist_ok=True)
for root, dirs, files in os.walk(output_dir, topdown=False):
    [os.remove(os.path.join(root, f)) for f in files]
    [os.rmdir(os.path.join(root, d)) for d in dirs]

so = rt.SessionOptions()
EP_list = ['TIDLCompilationProvider','CPUExecutionProvider']
sess = rt.InferenceSession(onnx_model_path ,providers=EP_list, provider_options=[compile_options, {}], sess_options=so)

input_details = sess.get_inputs()
for num in tqdm.trange(len(calib_images)):
    output = list(sess.run(None, {input_details[0].name : preprocess(calib_images[num])}))[0]

##optional
#subgraph_link =get_svg_path(output_dir) 
#for sg in subgraph_link:
#    hl_text = os.path.join(*Path(sg).parts[4:])
#    sg_rel = os.path.join('../', sg)
#    display(md("[{}]({})".format(hl_text,sg_rel)))
#
#EP_list = ['TIDLExecutionProvider','CPUExecutionProvider']
#print("[ken debug] 5 ")
#sess = rt.InferenceSession(onnx_model_path ,providers=EP_list, provider_options=[compile_options, {}], sess_options=so)
##Running inference several times to get an stable performance output
#for i in range(5):
#    output = list(sess.run(None, {input_details[0].name : preprocess('sample-images/elephant.bmp')}))
#
#for idx, cls in enumerate(output[0].squeeze().argsort()[-5:][::-1]):
#    print('[%d] %s' % (idx, '/'.join(imagenet_class_to_name(cls))))
#    
#from scripts.utils import plot_TI_performance_data, plot_TI_DDRBW_data, get_benchmark_output
#stats = sess.get_TI_benchmark_data()
#fig, ax = plt.subplots(nrows=1, ncols=1, figsize=(10,5))
#plot_TI_performance_data(stats, axis=ax)
#plt.show()
#print("[ken debug] 6 ")
#tt, st, rb, wb = get_benchmark_output(stats)
#print(f'Statistics : \n Inferences Per Second   : {1000.0/tt :7.2f} fps')
#print(f' Inference Time Per Image : {tt :7.2f} ms  \n DDR BW Per Image        : {rb+ wb : 7.2f} MB')

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、请检查两件事。

    1.确保您的 /tidl_tools/是否存在、并且具有以下版本。

    tidl_tools$ ls -1
    device_config.cfg
    ignore.log
    itidl_rt.h
    itvm_rt.h
    libtidl_onnxrt_ep.so
    libtidl_TFL_Delegate.so
    libvx_tidl_rt.so
    libvx_tidl_rt.SO.1.0
    nc_infofile.txt
    netbufinfo.bin
    osrt_deps
    PC_DSP_TEST_dl_algo.out
    ti_cnnperfsim.out
    tidl_graphVisualizer.out
    tidl_graphVisualizer_runtimes.out
    tidl_model_import_onnx.so
    tidl_model_import.out
    tidl_model_import_relay.so
    tidl_model_import.so
    tidl_model_import_tflite.so
    tidl_model_secure.out
    version.txt

    如果没有、请将 SOC 设置到您的器件、并从 edgeai-tidl-tools/目录中运行"source ./setup.sh"(这会需要一些时间)。

    2.如果 存在 edgeai-tidl-tools/tidl_tools 并且该文件具有上述文件、则设置 tidl_tools_path=/  /edgeai-tidl-tools/tidl_tools.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好:

    我检查下面的 tidl_tools 文件、该文件正确(SOC = am67a)

    并且已将 TIDL_TOOLS_PATH 设置为 tidl_tools 的完整路径

    我的 TIDL 版本是10.00.04.00、可在 PC (Ubuntu 22.04)上运行

    请帮助我检查、

    感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请尝试以下操作:

    更改:

     scripts.utils 导入 loggerWritter log_dir
    
     = Path ("logs").mkdir (parents=True、exists_ok=True)
    
    # stdout 和 stderr 保存到*。log 文件。 
    通过 loggerWritter ("logs/custon-model-onnx"): 
    
    #模型编译选项 


    以粗体添加行:

     scripts.utils 导入 loggerWritter log_dir
    
     = Path ("logs").mkdir (parents=True、exist_ok=True) 
    打印(os.environon['tidl_tools_path']) 
    # stdout 和 stderr 已保存到*。log 文件中。 
    通过 loggerWritter ("logs/custon-model-onnx"):
    #模型编译选项


    确保输出的值
    os.environ['tidl_tools_path'] 匹配您的 tidl_tools/目录 . 应该是这样
    指向 edgeai-tidl-tools/tidl_tools/目录。
    否则、您可能在设置变量之前启动了"jupyter 笔记本"。

    或者、如果您想要更多控制 jupyter 笔记本、您可以从运行模型
    edgeai-tidl-tools/example/osrt_python/ort/中的命令行方式:

    python3 ./onnxrt_ep.py -m cl-ort-resnet18-v1 -c (首先编译模型)
    python3 ./ onnxrt_ep.py -m cl-ort-resnet18-v1 -d (在 x86处理器上运行模型) 

    python3 ./onnxrt_ep.py -m cl-ort-resnet18-v1 (使用 C7x 仿真在 PC 上运行模型)
     
     
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好:

    我打印  os.environ['tidl_tools_path']、   路径似乎正确。

    感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好!

    我尝试运行命令 python3 ./onnxrt_ep.py -m cl-ort-resnet18-v1 -c

    并遇到以下错误:AttributeError: 'InferenceSession' object has no attribute 'get_TI_benchmark_data'

    这可能是因为TIDLCompilationProvider未使用?

    感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您正在运行哪个版本的 TIDL? 我会推荐10.0变体。  看起来您是从 Docker 容器运行此程序的;正确吗?  您是否可以从容器外部运行它来消除一些差异?   

    我确定这 可以正常工作、因此我唯一能想到的是重新安装 tidl_tools。  要执行此操作、请移动/删除 tidl_tools (重新安装时不应存在该目录)。  确保已设置 SOC 并从 edgeai-tidl-tools 目录运行"source ./setup.sh"。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好:

    我运行 TIDL 版本10.00.04.00。  

    是的、我从 Docker 容器运行此文件。

    非常感谢您的建议。 我将尝试直接在 Ubuntu 系统上运行它、而不使用容器。 此外、我是否可以确认 SOC 是否应设置为"am67a"?

    感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Ken:

    am67a 正确。   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好:

    我想仔细检查我遵循的步骤、以确保它们正确无误:

    [ENV]

    不带容器

    第二百零四章

    TIDL:10.00.04.00

    [步骤]

    1. Export SOC=am67a
    2. 资料来源:setup.sh
    3. Export tidl_tools_path=$(pwd)/tidl_tools
      导出 LD_LIBRARY_PATH=$LD_LIBRARY_PATH:$TIDL_TOOLS_PATH
      Export arm64_gcc_path=$(pwd)/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu
    4. cd examples/jupyter_notebook
    5. 资料来源:launch_notebook.sh
    6. EXEC custom-model-onnx.ipynb

    请确认这些步骤是否正确吗?

    此外、我想问一下输出文件是否位于custom-artifacts/onnx/笔记本中指定的目录中?

    感谢您的帮助!

    此致、

    Ken

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Ken:

    我运行了你的所有步骤,但我对你如何运行 jupyter ipynb 文件感到困惑。   我使用的是 Ubuntu 22.04、而 exec 不起作用。  您是如何运行它的? 我听说过使用  papermill 从命令行运行笔记本、但 exec 没有任何作用。   

    Chris

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好:

    我将 Jupyter Notebook 文件中的代码复制到一个.py文件并使用 Python 3执行。

    感谢您的帮助!

    此致、

    Ken

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、您好:

    我尝试在没有容器的情况下运行 TIDL、onnx 转换工具可以起作用、

    但我从获得了新问题   

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1446866/processor-sdk-j722s-tidl-convert-custom-onnx-model-to-tidl-format-fail 

    和  

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1446870/processor-sdk-j722s-tidl-convert-default-onnx-tflite-model-to-tidl-format-fail

    感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请为此使用其他主题帖。  我将关闭该主题帖。