This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
您好!
在向 DSP 添加一些小算法之后(C6x_1 CPU:20%)、
图像闪烁发生在 camera->video->DSS 中。
1.这可能吗?
?可以禁用 C6x_1/2 μ s 的 TIOVX 功能
谢谢
东张
您好!
对音频 μ、 使用1个 C66、并使用 IPC。
C66_1和 C66_2都具有 func、
#if defined(x86_64) || defined(C66) void tivxRemoveTargetKernelDLColorConvert(void); #endif static Tivx_Target_Kernel_List gTivx_target_kernel_list[] = { {&tivxAddTargetKernelOCPreProc, &tivxRemoveTargetKernelOCPreProc}, {&tivxAddTargetKernelOCPostProc, &tivxRemoveTargetKernelOCPostProc}, {&tivxAddTargetKernelPoseViz, &tivxRemoveTargetKernelPoseViz}, {&tivxAddTargetKernelDrawKeypointDetections, &tivxRemoveTargetKernelDrawKeypointDetections}, {&tivxAddTargetKernelDrawBoxDetections, &tivxRemoveTargetKernelDrawBoxDetections}, {&tivxAddTargetKernelDLPreProc, &tivxRemoveTargetKernelDLPreProc}, {&tivxAddTargetKernelDLColorBlend, &tivxRemoveTargetKernelDLColorBlend}, {&tivxAddTargetKernelDLDrawBox, &tivxRemoveTargetKernelDLDrawBox}, {&tivxAddTargetKernelImgPreProc, &tivxRemoveTargetKernelImgPreProc}, {&tivxAddTargetKernelPixelViz, &tivxRemoveTargetKernelPixelViz}, {&tivxAddTargetKernelODPostProc, &tivxRemoveTargetKernelODPostProc}, {&tivxAddTargetKernelDofPlaneSep, &tivxRemoveTargetKernelDofPlaneSep}, {&tivxAddTargetKernelVisualLocalization, &tivxRemoveTargetKernelVisualLocalization}, #if defined(x86_64) || defined(C66) {&tivxAddTargetKernelDLColorConvert, &tivxRemoveTargetKernelDLColorConvert}, #endif };
能否在 C66_2中删除这些函数而不影响视觉应用?
谢谢
东张
您好!
是的、如果您不使用此功能、则删除相同的功能。
此外、如果您未将 C66x 内核用于 vision_apps、您可以通过以下2个步骤删除整个内容。
步骤1:中 vision_apps/platform/j721e/rtos/common/app_cfg.h、 您可以注释掉 ENABLE_IPC_C66x_1和2
步骤2:中 SDK_builder/vision_apps_build_flags.mak 您可以将 BUILD_CPU_C6x_1和2更改为"NO"
这样、VISION_APPS 二进制文件不会连接到 C66x 内核
此致、
Nikhil