This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4AL-Q1:用于连接 MAX96789串行器的 DSS 设置

Guru**** 2482225 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1442027/tda4al-q1-dss-setting-to-connect-max96789-serializer

器件型号:TDA4AL-Q1

工具与软件:

尊敬的 Champs,

我的客户正在尝试通过 DSI 将 MAX96789连接到 DSS 端口0、但通过 MAX96789没有显示。

您能否检查以下设置是否可以显示?

PRM.timings.width = 1920U;
prm.timings.height = 1080U;
prm.timings.hFrontPorch = 8U;
prm.timings.hBackPorch = 40U;
prm.timings.hSyncLen = 32U;
prm.timings.vFrontPorch = 17U;
prm.timings.vBackPorch = 6U;
prm.timings.vSyncLen = 8U;
crm.timings.pixelClock = 133320000ULL;
FPS = 60
通道= 4
通道速度(Kbps)= 416625U

它们的时钟源为 OSC0 = 19.2M、OSC1 = 26M、如下所示。

谢谢、此致、

SI