This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM6442:了解捕获的 PPS 时间戳

Guru**** 2018070 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1454597/am6442-making-sense-of-captured-pps-timestamps

器件型号:AM6442

工具与软件:

大家好!

我已将 PTP 时钟设置为 UTC。

sudo phc_ctl /dev/ptp0获取
PHC_ctl[54489.791]:时钟时间为1734773436.940368982或2024年12月21日09:30:36


每隔启用 PPS 后、CAPR6会发生变化、我将获得如下值:

REG0 => 0x1ca1b6
REG1 = 0x2044b8

我如何理解这些值?

当 CAPR6更改时、我在 CAP 状态寄存器中获得以下信息:


'CAP_VALID':'0b1110000000'

'CAP_RAW':'0b11000000'

看起来正常吗? 我无法理解表中的最后一项。 "树"是什么意思? 此致。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    CAP_VALID 没有详细记录、位10是0至9范围内所有有效位的 OR

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    设法获得更好的时间戳。

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    #include <stdint.h>
    #include "./Dependencies/intc_map_0.h"
    #include "./Dependencies/resource_table.h"
    #include "./pru_registers.h" // __R30 and __R31, avoid IDE warnings.
    #define SHARED_ICSSG_MEM (0x10000)
    volatile uint32_t *icssg_shared_mem_ = (uint32_t *)SHARED_ICSSG_MEM;
    void HW_WR_REG32(uint32_t addr, uint32_t value) {
    *(volatile uint32_t *)((uintptr_t)addr) = value;
    }
    inline void pad_config_aka_dtb() {
    HW_WR_REG32(0x00a40034, 0x010016);
    HW_WR_REG32(0x00a40038, 0x010016);
    HW_WR_REG32(0x00a4003C, 0x010016);
    HW_WR_REG32(0x00a40040, 0x010016);
    // pin mux for LATCH_IN - time sync router PRG1_IEP0_EDC_LATCH_IN0
    HW_WR_REG32(0x000F4100, 0x00040002);
    // time sync router PRG1_IEP0_EDC_LATCH_IN1
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    这是我用于处理后面的日志的程序。

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    #include <iostream>
    #include <fcntl.h>
    #include <sys/mman.h>
    #include <unistd.h>
    #include <cstdint>
    int main(){
    const size_t PAGE_SIZE = sysconf(_SC_PAGE_SIZE);
    const off_t BASE_ADDR = 0x30090000 & ~(PAGE_SIZE - 1);
    int fd = open("/dev/mem", O_RDONLY | O_SYNC);
    void* map = mmap(NULL, PAGE_SIZE, PROT_READ, MAP_SHARED, fd, BASE_ADDR);
    volatile uint32_t* mem = (volatile uint32_t*)map;
    auto off = (0x30090000 - BASE_ADDR) / sizeof(uint32_t);
    uint32_t prevVal = 0xFFFFFFFF;
    uint64_t prevCount = 0;
    while(true){
    uint32_t val = mem[off];
    if(val != prevVal){
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    如果在未连接 PTP 服务器的情况下运行、捕获的寄存器将以每秒250m 的增量(如果将时钟间隔乘以4ns、则为1S)。

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    mem0x0Count: 0, mem0x8R0: 8399040269, Diff: 8399040269
    mem0x0Count: 1, mem0x8R0: 570425132, Diff: 18446744065880936479
    mem0x0Count: 2, mem0x8R0: 820425132, Diff: 250000000
    mem0x0Count: 3, mem0x8R0: 1070425132, Diff: 250000000
    mem0x0Count: 4, mem0x8R0: 1320425132, Diff: 250000000
    mem0x0Count: 5, mem0x8R0: 1570425132, Diff: 250000000
    mem0x0Count: 6, mem0x8R0: 1820425132, Diff: 250000000
    mem0x0Count: 7, mem0x8R0: 2070425132, Diff: 250000000
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

     

    启动 PTP 客户端后、我会得到时间戳之间的不同增量。

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    mem0x0Count: 147, mem0x8R0: 36771615672, Diff: 250001539
    mem0x0Count: 148, mem0x8R0: 37021617218, Diff: 250001546
    mem0x0Count: 149, mem0x8R0: 37271618771, Diff: 250001553
    mem0x0Count: 150, mem0x8R0: 37521620320, Diff: 250001549
    mem0x0Count: 151, mem0x8R0: 37771621871, Diff: 250001551
    mem0x0Count: 152, mem0x8R0: 38021623426, Diff: 250001555
    mem0x0Count: 153, mem0x8R0: 38271624987, Diff: 250001561
    mem0x0Count: 154, mem0x8R0: 38521626543, Diff: 250001556
    mem0x0Count: 155, mem0x8R0: 38771628098, Diff: 250001555
    mem0x0Count: 156, mem0x8R0: 39021629642, Diff: 250001544
    mem0x0Count: 157, mem0x8R0: 39271631184, Diff: 250001542
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    我理解的是、从我们的角度来看、主站的1S 对于我们而言大约为1000006316ns、因此我们的速度较慢。

    这是我在 ptp4l 日志中看到的内容。 这看起来非常像频率调整过程。

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    ptp4l[1454.315]: master offset 9 s2 freq +6358 path delay 409
    ptp4l[1455.315]: master offset -58 s2 freq +6293 path delay 410
    ptp4l[1456.316]: master offset -59 s2 freq +6275 path delay 410
    ptp4l[1457.316]: master offset 6 s2 freq +6322 path delay 410
    ptp4l[1458.316]: master offset 32 s2 freq +6350 path delay 407
    ptp4l[1459.316]: master offset 37 s2 freq +6365 path delay 410
    ptp4l[1460.316]: master offset 54 s2 freq +6393 path delay 408
    ptp4l[1461.316]: master offset 12 s2 freq +6367 path delay 408
    ptp4l[1462.316]: master offset 17 s2 freq +6376 path delay 407
    ptp4l[1463.316]: master offset -28 s2 freq +6336 path delay 407
    ptp4l[1464.316]: master offset -70 s2 freq +6285 path delay 409
    ptp4l[1465.316]: master offset -67 s2 freq +6267 path delay 409
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    我想现在这是有道理的。 希望。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    对于 主站、1s 约为1s+6.3us、因此我们较慢。 (我试图编辑上面的帖子,但它不起作用)。