This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM6442:了解捕获的 PPS 时间戳

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1454597/am6442-making-sense-of-captured-pps-timestamps

器件型号:AM6442

工具与软件:

大家好!

我已将 PTP 时钟设置为 UTC。

sudo phc_ctl /dev/ptp0获取
PHC_ctl[54489.791]:时钟时间为1734773436.940368982或2024年12月21日09:30:36


每隔启用 PPS 后、CAPR6会发生变化、我将获得如下值:

REG0 => 0x1ca1b6
REG1 = 0x2044b8

我如何理解这些值?

当 CAPR6更改时、我在 CAP 状态寄存器中获得以下信息:


'CAP_VALID':'0b1110000000'

'CAP_RAW':'0b11000000'

看起来正常吗? 我无法理解表中的最后一项。 "树"是什么意思? 此致。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    CAP_VALID 没有详细记录、位10是0至9范围内所有有效位的 OR

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    设法获得更好的时间戳。

    #include <stdint.h>
    
    #include "./Dependencies/intc_map_0.h"
    #include "./Dependencies/resource_table.h"
    #include "./pru_registers.h"  // __R30 and __R31, avoid IDE warnings.
    
    #define SHARED_ICSSG_MEM (0x10000)
    volatile uint32_t *icssg_shared_mem_ = (uint32_t *)SHARED_ICSSG_MEM;
    
    void HW_WR_REG32(uint32_t addr, uint32_t value) {
      *(volatile uint32_t *)((uintptr_t)addr) = value;
    }
    
    inline void pad_config_aka_dtb() {
      HW_WR_REG32(0x00a40034, 0x010016);
      HW_WR_REG32(0x00a40038, 0x010016);
      HW_WR_REG32(0x00a4003C, 0x010016);
      HW_WR_REG32(0x00a40040, 0x010016);
      // pin mux for LATCH_IN - time sync router PRG1_IEP0_EDC_LATCH_IN0
      HW_WR_REG32(0x000F4100, 0x00040002);
      //  time sync router PRG1_IEP0_EDC_LATCH_IN1
      HW_WR_REG32(0x00a40028, 0x00010009);
    }
    
    void reset_counter_iep_iep1() {
      /* Disable counter */
      CT_IEP1.global_cfg_reg_bit.cnt_enable = 0;
      /* 64 bits? */
      CT_IEP1.cmp_cfg_reg_bit.shadow_en = 0;
      /* Reset Count register */
      CT_IEP1.count_reg0_bit.count_lo = 0xFFFFFFFF;
      CT_IEP1.count_reg1_bit.count_hi = 0xFFFFFFFF;
      /* Clear overflow status register */
      CT_IEP1.global_status_reg_bit.cnt_ovf = 1;
    }
    
    void configure_counter_iep1() {
      CT_IEP1.cmp_cfg_reg_bit.cmp_en = 0;
      CT_IEP1.compen_reg_bit.compen_cnt = 0;
      CT_IEP1.global_cfg_reg_bit.default_inc = 1;
      CT_IEP1.global_cfg_reg_bit.cnt_enable = 1;
    }
    
    void main() {
      pad_config_aka_dtb();
      reset_counter_iep_iep1();
      configure_counter_iep1();
    
      CT_IEP1.cap_cfg_reg = 0x0003FFC0;
    
      uint32_t reg0 = CT_IEP1.capr6_reg0;
      uint32_t reg1 = CT_IEP1.capr6_reg1;
      uint32_t reg2 = CT_IEP1.cap_status_reg;
    
      *(icssg_shared_mem_) = 0;
      *(icssg_shared_mem_ + 2) = reg0;
      *(icssg_shared_mem_ + 3) = reg1;
    
      while (1) {
        reg2 = CT_IEP1.cap_status_reg;
        reg0 = CT_IEP1.capr6_reg0;
        reg1 = CT_IEP1.capr6_reg1;
    
        if ((*(icssg_shared_mem_ + 2) != reg0 ||
             (*(icssg_shared_mem_ + 3) != reg1))) {
          *(icssg_shared_mem_ + 4) = reg2;
    
          *(icssg_shared_mem_) += 1;
          *(icssg_shared_mem_ + 2) = reg0;
          *(icssg_shared_mem_ + 3) = reg1;
        }
      }
    }
    

    这是我用于处理后面的日志的程序。

    #include <iostream>
    #include <fcntl.h>
    #include <sys/mman.h>
    #include <unistd.h>
    #include <cstdint>
    
    int main(){
        const size_t PAGE_SIZE = sysconf(_SC_PAGE_SIZE);
        const off_t BASE_ADDR  = 0x30090000 & ~(PAGE_SIZE - 1);
        int fd = open("/dev/mem", O_RDONLY | O_SYNC);
        void* map = mmap(NULL, PAGE_SIZE, PROT_READ, MAP_SHARED, fd, BASE_ADDR);
    
        volatile uint32_t* mem = (volatile uint32_t*)map;
        auto off = (0x30090000 - BASE_ADDR) / sizeof(uint32_t);
    
        uint32_t prevVal = 0xFFFFFFFF; 
        uint64_t prevCount = 0;
    
        while(true){
            uint32_t val = mem[off];
            if(val != prevVal){
                uint64_t low  = mem[off + 2]; 
                uint64_t high = mem[off + 3];
                uint64_t cnt  = (high << 32) | low;
                std::cout << "mem0x0Count: " << val
                          << ", mem0x8R0: "   << cnt
                          << ", Diff: "       << (cnt - prevCount)
                          << std::endl;
                prevVal   = val;
                prevCount = cnt;
            } else usleep(50000);
        }
    
        munmap(map, PAGE_SIZE);
        close(fd);
        return 0;
    }
    

    如果在未连接 PTP 服务器的情况下运行、捕获的寄存器将以每秒250m 的增量(如果将时钟间隔乘以4ns、则为1S)。

    mem0x0Count: 0, mem0x8R0: 8399040269, Diff: 8399040269
    mem0x0Count: 1, mem0x8R0: 570425132, Diff: 18446744065880936479
    mem0x0Count: 2, mem0x8R0: 820425132, Diff: 250000000
    mem0x0Count: 3, mem0x8R0: 1070425132, Diff: 250000000
    mem0x0Count: 4, mem0x8R0: 1320425132, Diff: 250000000
    mem0x0Count: 5, mem0x8R0: 1570425132, Diff: 250000000
    mem0x0Count: 6, mem0x8R0: 1820425132, Diff: 250000000
    mem0x0Count: 7, mem0x8R0: 2070425132, Diff: 250000000
    

     

    启动 PTP 客户端后、我会得到时间戳之间的不同增量。

    mem0x0Count: 147, mem0x8R0: 36771615672, Diff: 250001539
    mem0x0Count: 148, mem0x8R0: 37021617218, Diff: 250001546
    mem0x0Count: 149, mem0x8R0: 37271618771, Diff: 250001553
    mem0x0Count: 150, mem0x8R0: 37521620320, Diff: 250001549
    mem0x0Count: 151, mem0x8R0: 37771621871, Diff: 250001551
    mem0x0Count: 152, mem0x8R0: 38021623426, Diff: 250001555
    mem0x0Count: 153, mem0x8R0: 38271624987, Diff: 250001561
    mem0x0Count: 154, mem0x8R0: 38521626543, Diff: 250001556
    mem0x0Count: 155, mem0x8R0: 38771628098, Diff: 250001555
    mem0x0Count: 156, mem0x8R0: 39021629642, Diff: 250001544
    mem0x0Count: 157, mem0x8R0: 39271631184, Diff: 250001542

    我理解的是、从我们的角度来看、主站的1S 对于我们而言大约为1000006316ns、因此我们的速度较慢。

    这是我在 ptp4l 日志中看到的内容。 这看起来非常像频率调整过程。

    ptp4l[1454.315]: master offset          9 s2 freq   +6358 path delay       409
    ptp4l[1455.315]: master offset        -58 s2 freq   +6293 path delay       410
    ptp4l[1456.316]: master offset        -59 s2 freq   +6275 path delay       410
    ptp4l[1457.316]: master offset          6 s2 freq   +6322 path delay       410
    ptp4l[1458.316]: master offset         32 s2 freq   +6350 path delay       407
    ptp4l[1459.316]: master offset         37 s2 freq   +6365 path delay       410
    ptp4l[1460.316]: master offset         54 s2 freq   +6393 path delay       408
    ptp4l[1461.316]: master offset         12 s2 freq   +6367 path delay       408
    ptp4l[1462.316]: master offset         17 s2 freq   +6376 path delay       407
    ptp4l[1463.316]: master offset        -28 s2 freq   +6336 path delay       407
    ptp4l[1464.316]: master offset        -70 s2 freq   +6285 path delay       409
    ptp4l[1465.316]: master offset        -67 s2 freq   +6267 path delay       409

    我想现在这是有道理的。 希望。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    对于 主站、1s 约为1s+6.3us、因此我们较慢。 (我试图编辑上面的帖子,但它不起作用)。