This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [常见问题解答] J784S4XEVM:如何在 eMMC 中配置 PSLC

Guru**** 2551110 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1469551/faq-j784s4xevm-how-to-configure-pslc-in-emmc

器件型号:J784S4XEVM

工具与软件:

尊敬的 Gokul:

您能帮助我在 eMMC 中配置 PSLC 吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Gokul:

    参考主题:

    e2e.ti.com/.../tda4vl-q1-mmcsd-driver-set-pslc-mode-for-emmc

    使用 mcu-util 在 Linux 内核中配置 PSLC:

    命令 :[ MMC ENH_AREA --help ]命令。

    在 uboot 中配置 PSLC:

    1:进入 Linux 内核,执行以下命令,只需记下它:

      > cat /sys/class/block/mmcblk0/size

      它基本上表示 eMMC uda 分区中存在的512个块的数量

    2:重新引导至 Uboot 和 e nter the below command which will just test if it is working:

    > mmc hwpartition user enh <start> <number of 512B sized blocks> check

    SYNTAX:



    I am attaching an example below just for reference:

    Here 62160896 is the value obtained after running cat /sys/class/block/mmcblk0/size as stated earlier.

    Here 1264 indicates the maximum number of HC WP Group Size(8Mib(as in the below image)) blocks allowed.

    Hence number of 512B sized blocks now = (1264×8×1024×1024)/512 which is equal to 20709376 which works fine.


    3:Now to set this configuration permanently:
    NOTE:Because all the operations are one-time only,be very careful before applying the below command.
     > mmc hwpartition user enh 0 20709376 wrrel on complete

    4:Power cycle the board for the changes to get applied.

    Regards
    Gokul