This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:从 PC 启动 AFE 时出现问题

Guru**** 2928980 points

Other Parts Discussed in Thread: AFE7950EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1647826/afe7950evm-issue-with-bringing-afe-up-from-pc

器件型号: AFE7950EVM

大家好,我在前面的问题中已经提到过,我们尝试使用 Latte 的(1G BW 设计)对 AFE 进行编程。 我们能够顺利获得射频。 当我们使用 Latte 生成的日志文件从 PC 执行此操作时、便能够像这样正确地在 NCO 处获取射频

 但是、当我们将射频从 NCO 移出、然后频谱变得糟糕时、不需要的信号会从中心频率到达+/- 375MHz。 随着本底噪声也在变化。 我们不确定为什么会发生这些事情。

我将从 Latte 创建的 AFE 脚本和日志文件附加到您的参考中。 请告诉我们这一问题的含义。 谢谢你。

Afe79xxPg1.txt LMKCommands.txt AFECommands.txt 

sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion

setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro 
##############		Top Level			##############
sysParams.FRef			= 500 #404.2#500
sysParams.FadcRx		= 3000 #2425.2 #3000
sysParams.FadcFb		= 3000 #2425.2 #3000
sysParams.Fdac			= 3000*4 #2425.2*4 # 3000*4
sysParams.externalClockRx=False
sysParams.externalClockTx=False
sysParams.RRFMode		= 5					# RRF 0: 4T4R2F FDD Mode
sysParams.enableDacInterleavedMode=False
													
##############		Digital Chain		##############

		#####	RX	#####
sysParams.rxEnable = [True,False,False,False]
sysParams.ddcFactorRx	=	[2]*4					#DDC decimation factor for RX A, B, C and D
sysParams.rxNco0		= 	[[3750,3750],			#Band0, Band1 for RXA 
							[9750,9750],        	#Band0, Band1 for RXB 
							[9750,9750],        	#Band0, Band1 for RXC 
							[9750,9750]]        	#Band0, Band1 for RXD 

		#####	FB	#####
sysParams.ddcFactorFb	=	[3]*2					#DDC decimation factor for FB 1 and 2
sysParams.fbNco0		= 	[9750,9750]				#Band0 for FB1 and FB2 
sysParams.fbEnable		=	[False,False]

		#####	TX	#####
sysParams.txEnable = [True,False,False,False]
sysParams.ducFactorTx	=	[8]*4					#DUC interpolation factor for TX A, B, C and D
sysParams.txNco0		= 	[[3750,3750],			#Band0, Band1 for TXA 
							[9750,9750],        	#Band0, Band1 for TXB 
							[9750,9750],        	#Band0, Band1 for TXC 
							[9750,9750]]        	#Band0, Band1 for TXD 



##############		JESD		##############

		#####	ADC-JESD	#####
sysParams.jesdSystemMode= [3,3]
													#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb -fb
													#SystemMode 1:	1R1F-FDD						; rx -rx -fb -fb
													#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
													#SystemMode 3:	1R								; rx -rx -rx -rx
													#SystemMode 4:	1F								; fb -fb- fb -fb
													#SystemMode 5:	1R1F-TDD						; rx/fb-rx/fb-rx/fb-rx/fb
													
sysParams.jesdTxProtocol= [2,2]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
sysParams.LMFSHdRx		= ["42220"]*4
													# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
													# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb		= ["22210","22210"]

sysParams.rxJesdTxScr	= [False,False,False,False]
sysParams.fbJesdTxScr	= [False,False]

sysParams.rxJesdTxK		= [1,1,1,1]
sysParams.fbJesdTxK		= [1,1]
sysParams.serdesTxLanePolarity =[1,1,0,0,1,1,0,0]
sysParams.jesdTxLaneMux	= [1,0,3,2,4,5,6,7]			# Enter which lanes you want in each location. 
													# For example, if you want to exchange the first two lines of each 2T,
													#		this should be [[1,0,2,3],[5,4,6,7]]

		#####	DAC-JESD	#####
sysParams.jesdRxProtocol= [2,2]
sysParams.LMFSHdTx		= ["42220"]*4
sysParams.serdesRxLanePolarity=[1,1,1,1,0,0,0,0]
sysParams.jesdRxLaneMux	= [1,0,3,2,4,5,6,7]			# Enter which lanes you want in each location.
													# For example, if you want to exchange the first two lines of each 2R
													#		this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd		= [4, 4]
sysParams.jesdRxScr		= [False,False,False,False]
sysParams.jesdRxK		= [1,1,1,1]

		#####	JESD Common	#####
	
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack	= True	#JESD Sync signal is connected to FPGA

##############		GPIO		##############
sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'ADC_SYNC1',
						'N8': 'ADC_SYNC2',
						'N7': 'ADC_SYNC3',
						'H9': 'DAC_SYNC0',
						'G9': 'DAC_SYNC1',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}

##############		LMK Params		##############
lmkParams.pllEn			= False
lmkParams.inputClk		= 1500 #1212.6 #1500 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk	= True
setupParams.fpgaRefClk	= 187.5 #151.575 #187.5 # Should be equal to LaneRate/40 for TSW14J56

##############		Logging		##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat=0x01# to generate format5 file
logDumpInst.rewriteFile=1
lmk.logClassInst                    =logDumpInst
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1
lmk.rawWriteLogEn                    = 1

device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
sysParams.ncoFreqMode 				=  "FCW"  ##"1KHz" ##"FCW"

setupParams.skipLmk	=	False
AFE.initializeConfig()
lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq
lmkParams.lmkPulseSysrefMode = False
AFE.LMK.lmkConfig()
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    跟踪此查询、了解通过 PC 使用 Latte 生成的日志文件进行编程时 AFE7950EVM 的行为。  

    请分享一下您对此的意见吗?