This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:与 FFD 行为相关的 RRF 模式与抽取不兼容

Guru**** 2893300 points

Other Parts Discussed in Thread: AFE7950EVM, AFE7950

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1415805/afe7950evm-rrf-modes-related-with-ffd-behaviour-not-compatible-with-decimation

器件型号:AFE7950EVM
Thread 中讨论的其他器件: AFE7950

工具与软件:

早上好。

我们的团队正在尝试使用 Latte 软件配置连接到 TSW14J58的 AFE7950EVM 板。 我们希望对 ADC 进行配置、使一个块的 ADC 抽取值为3、另一个块的 ADC 抽取值为2、如数据表中所示的选项。

选择的系统模式为 rrfmode 0、其中 Rx、Tx 和 FB 处于 FDD 模式

但是、一旦 Latte 编译了配置、就 会返回错误消息"Current RX DDC Factor setting 在 FDD 模式下不受支持"。 查看 Latte 的 python 代码、可在软件上将该限制硬编码、其中表示当输出速率为1000和1500、ADC 采样率为3,000,2500或2000时、FFD 模式不可用。

这是为什么? 是否有办法在其他配置中实现类似行为?

预期行为如下:4Rx 和4Tx 无反馈、64b/66b、3600MHz 单频带、两个 ADC 输出速率为1000Msps、两个 ADC 输出速率为1500Msps、2个 DAC 输入速率为1000Msps、其他2个 DAC 输入速率为1500Msps。 为了避免 DAC 出现错误、我们设计中的有效 DAC 采样率将为6000和12000MSPS。

Latte 中使用的当前启动文件如下所示:

##############		Read me			##############
#In HSDC Pro DAC tab, Select AFE79xx_2x2TX_44210; Data Rate = 491.52M
#In HSDC Pro ADC tab, Select AFE79xx_2x2RX_24410; Data Rate = 245.76M ---> To capture 4 RX channels
#In HSDC Pro ADC tab, Select AFE79xx_1x2FB_44210; Data Rate = 491.52M ---> To capture 2 FB channels

sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion

setupParams.skipFpga = 0 # setup FPGA (TSW14J58)

##############		Top Level			##############
sysParams.FRef			= 491.52     # Recommended 2949.12/6 (interno o externo, ahora es interno)
sysParams.FadcRx		= 2949.12    # Dependen de si el reloj es interno o externo (ahora mismo es interno )
sysParams.FadcFb		= 2949.12    # Dependen de si el reloj es interno o externo (ahora mismo es interno )
sysParams.Fdac			= 2949.12*2  # Dependen de si el reloj es interno o externo (ahora mismo es interno )
sysParams.externalClockRx=False      # Dependen de si el reloj es interno o externo (ahora mismo es interno )
sysParams.externalClockTx=False      # Dependen de si el reloj es interno o externo (ahora mismo es interno) 
													
##############		Digital Chain		##############

sysParams.RRFMode		= 0					# FDD Mode. This is a typical FDD mode with 4TX, 4RX chains and 2 FB chains,
                                            # where all RX and FB chains have independent ADCs

sysParams.ncoFreqMode = "FCW"

# Its possible to configur number of NCO by band

		#####	RX	#####
sysParams.ddcFactorRx	=	[3,3,2,2]			    #DDC decimation factor for RX A, B, C and D
sysParams.numBandsRx    =   [0,0,0,0]   # Single band
# Rx A B BW 500MHz -> Relacion 1000/3000 Msps - 3
# Rx B C BW 1GHz   -> Relacion 1500/3000 Msps - 2  
sysParams.rxNco0		= 	[[3600,3600],			#Band0, Band1 for RXA (media entre 3.3-3.9 GHz)
							[3600,3600],        	#Band0, Band1 for RXB (media entre 3.3-3.9 GHz)
							[3600,3600],        	#Band0, Band1 for RXC 
							[3600,3600]]        	#Band0, Band1 for RXD 

		#####	FB	#####
sysParams.fbEnable		=	[False,False]
sysParams.ddcFactorFb	=	[3,3]					#DDC decimation factor for FB 1 and 2
sysParams.fbNco0		= 	[3600,3600]				#Band0 for FB1 and FB2 

		#####	TX	#####
sysParams.ducFactorTx	=	[6,6,4,4]			#DUC interpolation factor for TX A, B, C and D 
sysParams.numBandsTx    =   [0,0,0,0]   # Single band
sysParams.txNco0		= 	[[4450,3600],			#Band0, Band1 for TXA 
							[4450,3600],        	#Band0, Band1 for TXB 
							[4450,3600],        	#Band0, Band1 for TXC 
							[4450,3600]]        	#Band0, Band1 for TXD


##############		JESD		##############

		#####	ADC-JESD	#####
sysParams.jesdSystemMode= [3,3] # case where, FB is not needed and only both channels of the RX
                                # are to be treated as a single JESD mapper
													
sysParams.jesdTxProtocol= [2,2]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
sysParams.LMFSHdRx		= ["44210","44210","44210","44210"]
													
sysParams.LMFSHdFb		= ["22210","22210"]

sysParams.rxJesdTxScr	= [False,False,False,False]
sysParams.fbJesdTxScr	= [False,False]

sysParams.rxJesdTxK		= [1,1,1,1] # Multiblock para 64b - 1
sysParams.fbJesdTxK		= [1,1]     # Multiblock para 64b - 1

sysParams.jesdTxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location. 
													# For example, if you want to exchange the first two lines of each 2T,
													#		this should be [[1,0,2,3],[5,4,6,7]]

		#####	DAC-JESD	#####
sysParams.jesdRxProtocol= [2,2]
sysParams.LMFSHdTx		= ["44210","44210","44210","44210"]

sysParams.jesdRxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location.
													# For example, if you want to exchange the first two lines of each 2R
													#		this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd		= [4, 4]
sysParams.jesdRxScr		= [False,False,False,False]
sysParams.jesdRxK		= [1,1,1,1] # Multiblock para 64b - 1

		#####	JESD Common	#####
	
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack	= False	#JESD Sync signal is connected to FPGA

##############		GPIO		##############
sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'ADC_SYNC1',
						'N8': 'ADC_SYNC2',
						'N7': 'ADC_SYNC3',
						'H9': 'DAC_SYNC0',
						'G9': 'DAC_SYNC1',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}

##############		LMK Params		##############
lmkParams.pllEn			= True
lmkParams.inputClk		= 983.04 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk	= True
setupParams.fpgaRefClk	= 245.76 # 2949.12/12

##############		Logging		##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat=0x1 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1

device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
AFE.deviceBringup()

AFE.TOP.overrideTdd(15,0,15)	# bit-wise; 4R,0F,4T

希望有任何帮助。

感谢你能抽出时间。

Jose

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Jose:

    对于小于4的抽取值、必须使用 RRF = 5。

     

    对于您感兴趣的模式、我们通常不建议使用不同的抽取/内插值、因为这会使系统更加复杂。 您是否可以仅使用输出/输入速率为1500MSPS 的 ADC 和 DAC?

     

    此致!

     

    Camilo

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Camilo:

    感谢对抽取行为进行仔细检查。

    另一方面、选择 AFE7950的原因之一是能够通过2R2T1FB 块配置系统。 我们必须能够获得一个配置、其中一个块用于1000、另一个块用于1500。

    此致!

    Jose

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    下午好!

    是否有关于在同一配置中使用多个抽取/内插值的更新? 想要完成此配置的另一个原因是功耗。 如果所有系统都能在1500下工作、我知道这会增加一般功耗。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Jose:

    我们已通过电子邮件联系到、目前正在关闭此帖子。

    此致!

    Camilo