团队、客户在问 AWR1843 UART 是否可以支持3M 波特率?
他们无法在我们的文档中找到此信息。
谢谢
五
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Adrian、您好!
对我来说、问题不在于降低波特率;问题在于如何将波特率精确设置为3M。
要将波特率设置为3M、VCLK 需要为3MHz x 16 x (n+1)= 48MHz、96MHz .... 那么、其中 n = 0、1、2、...
如果您设置:
gMmwMssMCB.cfg.sysClockFrequency = MSS_SYS_VCLK; gMmwMssMCB.cfg.loggingBaudRate = 3000000;
without change the setting of the MSS_SYS_VCLK; 假设 MSS_SYS_VCLK = 50MHz、那么您只能得到波特率= 3125000。