This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AWR1843AOPEVM:AWR1843AOPEVM

Guru**** 2555630 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1164732/awr1843aopevm-awr1843aopevm

器件型号:AWR1843AOPEVM

大家好, 当我调试 dss_main.c 时,它 总是挂起在 SOC_init()函数上 ,而不是单击暂停,调试窗口如下图所示。 看起来是内存问题。 如何解决?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    王嘉晶、

    您能否确认您是否对演示进行了任何更改? 或者您是否构建了自定义应用?

    此致、
    Saswat Kumar

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     的、我对演示进行了一些更改,导致 L2存储器不足和编译失败、因此我们的软件工程师修改了 DSS_MMW_linker.cmd 以增加 L2存储器、修改如下:  

    /*----------------------------------------------------------------------------*/
    /* Linker Settings                                                            */
    --retain="*(.intvecs)"
    
    --stack_size=0x700
    
    /* Get around a CCS issue; real-specify libraries ref'd in the overlays below. */
    -ldsplib.ae64P
    -llibmmwavealg_xwr18xx.ae674
    -lmathlib.ae674
    -llibsoc_xwr18xx.ae674
    -llibmailbox_xwr18xx.ae674
    -llibmmwave_xwr18xx.ae674
    -llibedma_xwr18xx.ae674
    -l./src/sysbios/sysbios.ae674
    -l./Debug/configPkg/package/cfg/dss_mmw_pe674.oe674
    -llibcrc_xwr18xx.ae674
    -llibadcbuf_xwr18xx.ae674
    -lrts6740_elf.lib
    
    /*----------------------------------------------------------------------------*/
    /* Section Configuration                                                      */
    SECTIONS
    {
        systemHeap : {} >> L2SRAM_UMAP0 | L2SRAM_UMAP1
        .l2data : {} >> L2SRAM_UMAP0 | L2SRAM_UMAP1
    
        /* HSSRAM has output data from processing chain running on DSP */
        .demoSharedMem > HSRAM
    
        /* L3SRAM has code that is overlaid with data, so data must be
           marked uninitialized. Application can initialize this section
           using _L3data_* symbols defined below. Code should be written carefully as
           these are linker symbols (see for example e2e.ti.com/.../92002 ):
    
            extern far uint8_t _L3data_start; // the type here does not matter
            extern far uint8_t _L3data_size;  // the type here does not matter
    
            memset((void *)_symval(&_L3data_start), 0, (uint32_t) _symval(&_L3data_size));
        */
        .l3data: type=NOINIT, start(_L3data_start), size(_L3data_size), load=L3SRAM PAGE 1
    
        /* Bootloader cannot load L1DSRAM, make sure to mark as NOINIT */
        .l1data : type=NOINIT, load=L1DSRAM
    
        /* Currently bootloader does not allow loading in L1PSRAM because of supporting
           low power. Below fast code is loaded in L3SRAM but run from L1PSRAM. The copy-in
           is called during initialization phase and copy-out is not used but can be added when
           supporting low-power mode (where L1 contents are not retained).
         */
        .fastCode:
        {
            dsplib.ae64P(.text)
            libmmwavealg_xwr18xx.ae674(.text)
            mathlib.ae674(.text)
            dss_data_path.oe674 (.text:MmwDemo_interFrameProcessing)
            dss_data_path.oe674 (.text:MmwDemo_processChirp)
            dss_data_path.oe674 (.text:MmwDemo_interChirpProcessing)
            dss_main.oe674 (.text:MmwDemo_dssDataPathProcessEvents)
            /* Below may be risky to expose hence currently hiding */
            // libosal_xwr16xx.ae674 (.text:SemaphoreP_pend)
            // libosal_xwr16xx.ae674 (.text:SemaphoreP_post)
            rts6740_elf.lib (.text:cos)
            rts6740_elf.lib (.text:sin)
            rts6740_elf.lib (.text:log)
            rts6740_elf.lib (.text:asin)
            rts6740_elf.lib (.text:expf)
        } load=L3SRAM PAGE 0, run=L1PSRAM PAGE 0, table(_MmwDemo_fastCode_L1PSRAM_copy_table, compression=off)
    
        /* This is auto generated by linker related to copy table above */
        .ovly > L2SRAM_UMAP0 | L2SRAM_UMAP1
    
        /* Overlay one-time/init-time (and non-critical in cycles) with L3 data,
           will be erased during data path processing. Note do not put any
           code that is required related to start/stop/reconfig processing */
        .overlay:
        {
            libsoc_xwr18xx.ae674 (.text:SOC_init)
            dss_main.oe674 (.text:MmwDemo_dssInitTask)
            dss_main.oe674 (.text:main)
            dss_data_path.oe674 (.text:MmwDemo_dataPathInitEdma)
    		libsoc_xwr18xx.ae674 (.text:SOC_deviceInit)
        } > L3SRAM PAGE 0
    
        .text_l3:
        {
            dss_main.oe674 (.text:MmwDemo_dssDataPathInit)
        } > L3SRAM PAGE 0
    
        .text_l3p1:
        {
        	dss_main.oe674 (.text:MmwDemo_parseProfileAndChirpConfig)
        	/*
        	libmailbox_xwr18xx.ae674 (.text)
        	dss_mmw_pe674.oe674 (.text:xdc_runtime_System_printfExtend__I)
        	sysbios.ae674 (.text)
        	*/
        	dss_mmw_pe674.oe674 (.text:xdc_runtime_System_printfExtend__I)
        	dss_main.oe674 (.text:MmwDemo_dssSendProcessOutputToMSS)
        	libcrc_xwr18xx.ae674 (.text:CRC_open)
        	libmailbox_xwr18xx.ae674 (.text:Mailbox_open)
        	libmmwave_xwr18xx.ae674 (.text:MMWave_initMMWaveLink)
        	libmmwave_xwr18xx.ae674 (.text:MMWave_startLink)
        	libedma_xwr18xx.ae674 (.text:EDMA_open)
        	dss_main.oe674 (.text:MmwDemo_parseAdcBufCfg)
        	libadcbuf_xwr18xx.ae674 (.text:ADCBUFCmdParamCheck)
        	libmmwave_xwr18xx.ae674 (.text:MMWave_flushCfg)
            libmmwave_xwr18xx.ae674 (.text:MMWave_getChirpHandle)
            libmmwave_xwr18xx.ae674 (.text:MMWave_start)
            libadcbuf_xwr18xx.ae674 (.text:ADCBUF_MMWave_open)
            dss_main.oe674 (.text:MmwDemo_dssDataPathConfigAdcBuf)
            libedma_xwr18xx.ae674 (.text:EDMA_init)
            dss_data_path.oe674 (.text:MmwDemo_dataPathConfigBuffers)
            libmmwave_xwr18xx.ae674 (.text:MMWave_init)
            dss_main.oe674 (.text:ODSDemo_objInit)
            libmailbox_xwr18xx.ae674 (.text:Mailbox_init)
            dss_data_path.oe674 (.text:MmwDemo_dataPathConfigEdma)
            dss_data_path.oe674 (.text:MmwDemo_dataPathConfigFFTs)
            libmmwave_xwr18xx.ae674 (.text:MMWave_initCRC)
            libmmwave_xwr18xx.ae674 (.text:MMWave_initLink)
            libadcbuf_xwr18xx.ae674 (.text:ADCBUF_MMWave_close)
            libmailbox_xwr18xx.ae674 (.text:Mailbox_close)
            dss_main.oe674 (.const:.string)
            sysbios.ae674 (.const:.string)
            dss_config_edma_util.oe674 (.const:.string)
            dss_data_path.oe674 (.const:.string)
            dss_mmw_pe674.oe674 (.const:.string)
        } > L3SRAM PAGE 1
    	
    }
    /*----------------------------------------------------------------------------*/

    请帮助您查看是否存在问题? 非常感谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Geogia、您好!

    除此之外、没有进行其他更改?

    此致、
    Saswat Kumar