请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:IWR1443 大家好、我有一个应用、其中有一个旋转盘、上面有目标、在转速为400rpm 时、目标距离可以是0.25英寸到0.5英寸。 IWR1443可支持的最小距离和最大速度是多少?
谢谢!
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.