请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LDC1101 您好!
客户正在设计 LDC 1101。
LDC 1101的基准输入频率最大值为16MHz。
使用外部振荡器(16MHz)时、可以使用多少 ppm?
客户估计约为±50ppm (16.08MHz)。
此致、
Sopatopa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
客户正在设计 LDC 1101。
LDC 1101的基准输入频率最大值为16MHz。
使用外部振荡器(16MHz)时、可以使用多少 ppm?
客户估计约为±50ppm (16.08MHz)。
此致、
Sopatopa