请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AWR1243 你好、冠军、
AWR1243/1642数据表中只有相位噪声@1MHz。 您能不能同时为76-77和77-81GHz 提供@1K、10K、100K 的值?
谢谢、
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.