请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:HDC1080 主题中讨论的其他器件: HDC2010
大家好、
根据数据表、在5°C ~60°C 时、温度传感器精度为+/-0.2°C
HDC1080在0°C 下是否保持+/-0.2°C 精度
或者、您能否帮助建议在0°C 下保持高精度的合适温度+湿度传感器?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.