请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TDC1000我需要一个 能够检测超过100m 深度的 AFE 器件。
TDC1000的测量范围高达8ms。
如果在水中、最大距离为12.4M (8/1000s * 1550M)。
我需要一个器件来实现超过100m 的传感。
如何使 AFE 设备检测超过100m?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.