请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LDC0851 用户指南指出、如果传感器和 LDC0851芯片之间的电缆连接长度超过2cm、则必须使用双绞线。 我的问题是、这是否意味着 LREF、LSENSE 和 LCOM 的3根电缆必须绞合? "双绞线"一词在某种程度上具有欺骗性、因为它应该是"双绞线"而不是3。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.