Other Parts Discussed in Thread: LDC1612
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:FDC2112 主题中讨论的其他器件:LDC1612
大家好、团队、
FDC 是否可以实现以下测量?
*晶圆平坦度检查
从传感器到晶圆的距离为14mm 或25mm
分辨率0.1mm
采样率150sps
此致、
特顿苏罗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.