Other Parts Discussed in Thread: UCC28C43
主题中讨论的其他器件:UCC28C43
Q15晶体管是否需要连接到电路中? 如果不是、该参数 Q15会产生什么负面影响?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UCC28C43
Q15晶体管是否需要连接到电路中? 如果不是、该参数 Q15会产生什么负面影响?
您好、Suma、
1)对于1)、当占空比超过50%时、需要斜坡补偿以抑制次谐波振荡。
通过实验调整组件值。 Q15是电压跟随器、R63为 Q15提供负载、选择1k 作为经验法则来偏置发射极电流。 C67是可选的(用于直流去耦)。 R71和 R72构成从 RT/CT 引脚到 CS 引脚的电阻分压器、R72的值越大、添加的补偿就越大。 R71的值在转换器以50V 输入运行的条件下进行调节、直到次谐波振荡消失。
2)对于2) C26和 C31、设置振荡器频率。 您可以在 UCC28C43数据表中检查计算结果以进行计算。

您好、Suma、
选择1000pF (1nF)时没有特别考虑、两者之间的任何值都是可以的。 1nF 是一个标准值可供选择。
斜率补偿公式根据 数据表第30页的公式(33)进行计算