This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
其思路是从交流发电机和整流器获取三相并将其调节为48VDC 输出、从而为系统提供航空电子设备。
在另一个方向上、蓄电池将为电机的交流发电机+起动器提供48VDC 电压。
AC2DC 建议包括:具有电桥3相(MOSFET)和换向器的整流器:
输入电压 40VDC- 400VDC。
输出电压48VDC。
输出电流100A。
换向器输出电压48VDC、电流输出100A。
读取电流和电压。
OVP、OCP、OTP 等
您好!
您似乎正在就基于 C2000的 TIDA-01606提出问题。 请在您的主题帖标题中包含 C2000、以便您的问题可以发送给正确的支持团队。 您当前的线程需要关闭。