This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-01604:f28379d

Guru**** 656470 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1166212/tida-01604-f28379d

器件型号:TIDA-01604

50Hz 频率的方波脉冲将根据以下所示的输入 PWM 模式被馈送到 GPIO、同时还会附加代码。问题出在脉冲的上升沿和下降沿。 如何解决此问题

#include "F28x_Project.h"
void InitEPwmTimer(void);
interrupt void xint1_isr(void);




void main(void)
{


    InitSysCtrl(); // Disable WD,init PLL,enable Peripheral Clocks
    DINT; //  Disable CPU interrupts
    /*Initialize the PIE control registers to their default state. The default state is all PIE interrupts disabled and flags
        are cleared*/
    InitPieCtrl();
    //      Disable CPU interrupts and clear all CPU interrupt flags:
    IER = 0x0000;   // Reset Interrupt Enable Register
    IFR = 0x0000;   // Reset Interrupt Flag Register
    InitPieVectTable();
    EALLOW;  // This is needed to write to EALLOW protected registers
       PieVectTable.XINT1_INT = &xint1_isr;

       EDIS;    // This is needed to disable write to EALLOW protected registers
       PieCtrlRegs.PIECTRL.bit.ENPIE = 1;          // Enable the PIE block
          PieCtrlRegs.PIEIER1.bit.INTx4 = 1;          // Enable PIE Gr

    InitEPwmTimer();    // For this example, only initialize the EPwm Timers

    IER |= M_INT1;    // Timer 0, ADC     // Enable CPU Interrupt 1

    EINT;                                 // Enable Global interrupt INTM
    ERTM;                                 // Enable Global real-time interrupt DBGM
    EALLOW;
       GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 0;         // GPIO
       GpioCtrlRegs.GPBDIR.bit.GPIO32 = 0;          // input
       GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 0;        // XINT1 Synch to SYSCLKOUT only
       EDIS;
       GPIO_SetupXINT1Gpio(32);
       XintRegs.XINT1CR.bit.POLARITY = 3;
       // Enable XINT1 and XINT2
       //
          XintRegs.XINT1CR.bit.ENABLE = 1;            // Enable XINT1

       //
          EALLOW;

               GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 0;        // GPIO
               GpioCtrlRegs.GPADIR.bit.GPIO19 = 1;         // output
             EDIS;

             while(1)
             {
  if(GpioDataRegs.GPBDAT.bit.GPIO32 == 1)      //  Data Register for this pin--Here rising edge is detected -this code works for Positive half cycle
                 {
      EALLOW;
      EPwm1Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
      EPwm1Regs.TZCTL.bit.TZA = 3;              // Do nothing
      EPwm1Regs.TZCTL.bit.TZB = 3;              // Do nothing
      EPwm3Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
       EPwm3Regs.TZCTL.bit.TZA = 3;              // Do nothing
       EPwm3Regs.TZCTL.bit.TZB = 3;              // Do nothing

      EPwm2Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
      EPwm2Regs.TZCTL.bit.TZA = 1;              //  Force EPWM2A to a high state
      EPwm2Regs.TZCTL.bit.TZB =1;              //Force EPWM2B to a high state

          EPwm4Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
          EPwm4Regs.TZCTL.bit.TZA = 1;              //  Force EPWM2A to a high state
          EPwm4Regs.TZCTL.bit.TZB =1;              //Force EPWM2B to a high state


              EDIS;
             EPwm2Regs.TBCTR = 0X0000;
             EPwm4Regs.TBCTR = 0X0000;
             EPwm1Regs.CMPA.bit.CMPA  = 5000;
             EPwm1Regs.CMPB.bit.CMPB  = 5000;
             EPwm3Regs.CMPA.bit.CMPA  = 5000;
             EPwm3Regs.CMPB.bit.CMPB  = 5000;



                 }
  else if (GpioDataRegs.GPBDAT.bit.GPIO32 == 0) //Here falling edge is detected -this code works for Negative half cycle
                 {
              EPwm1Regs.TBCTR = 0X0000;
              EPwm3Regs.TBCTR = 0X0000;
                   EALLOW;

              EPwm2Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
              EPwm2Regs.TZCTL.bit.TZA = 3;              // Do nothing
              EPwm2Regs.TZCTL.bit.TZB =3;              // Do nothing
              EPwm4Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
              EPwm4Regs.TZCTL.bit.TZA = 3;              // Do nothing
              EPwm4Regs.TZCTL.bit.TZB =3;              // Do nothing
                 EPwm1Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
              EPwm1Regs.TZCTL.bit.TZA = 1;              // Force EPWM1A to a high state
              EPwm1Regs.TZCTL.bit.TZB = 1;              // Force EPWM1B to a high state
              EPwm3Regs.TZFRC.bit.OST = 1;              // Force a one shot trip
                           EPwm3Regs.TZCTL.bit.TZA = 1;              // Force EPWM1A to a high state
                           EPwm3Regs.TZCTL.bit.TZB = 1;              // Force EPWM1B to a high state
                    EDIS;
               EPwm2Regs.CMPA.bit.CMPA  =5000;
               EPwm2Regs.CMPB.bit.CMPB  = 5000;
               EPwm4Regs.CMPA.bit.CMPA  =5000;
                             EPwm4Regs.CMPB.bit.CMPB  = 5000;

                 }
             }


}


  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    根据您的描述、很明显您没有收到所需的 PWM 输出。 在这之外、我不理解您在寻找什么。  

    我不知道该事件是何时发生的、您需要的效果是什么、或者您使用的是 TI 代码库。 如果您提供更多信息并提出特定问题、我可能会提供帮助。 如果不提供更多信息、我的建议是、输出可以改变、GPIO 多路复用器改变、动作限定符、死区、跳闸区、 数字比较可能都具有类似的效果、因此应进行检查。


    此致、
    Cody