请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53315 主题中讨论的其他器件:TINA-TI、
工具/软件:TINA-TI 或 Spice 模型
大家好、我遇到了 TPS53315无法达到预期输出电压的问题。 我的设计应该在12V 输入时达到0.9V 输出、但仿真不会超过0.6V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.