请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TIDA-00164
您好:
我的客户希望仔细检查6V_ISO 和18V_ISO 是否超出变压器(T1)的规格,因为他们喜欢在 此处找到 SEC 端5V/100mA (katalog.we-online.de/.../750342178.pdf)通知。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.