Other Parts Discussed in Thread: TIDA-00127, TPS40210
主题中讨论的其他器件: TPS40210
你(们)好
30W 超宽范围电源应能很好地满足我们的应用需求。 只需对方框图下第4页中的陈述进行一些澄清、"电源设计为输出保护继电器所需的行业标准电压"。 您是否有任何参考(IEC/EN/IEEE/等)、此行业标准电压来自哪里?.. 6.75V 输出使我感到困惑...
Rgds、
何塞
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TIDA-00127, TPS40210
你(们)好
30W 超宽范围电源应能很好地满足我们的应用需求。 只需对方框图下第4页中的陈述进行一些澄清、"电源设计为输出保护继电器所需的行业标准电压"。 您是否有任何参考(IEC/EN/IEEE/等)、此行业标准电压来自哪里?.. 6.75V 输出使我感到困惑...
Rgds、
何塞
你好 Jose
首先、感谢您关注 TIDA-00127。
电源设计为输出保护继电器所需的行业标准电压"。 您是否有任何参考(IEC/EN/IEEE/等)、此行业标准电压来自哪里?
我们必须更新保护继电器中常用电源轨的措辞、这些措辞为±12V、 5V 或15V 或24V。
我们将使用2A 负载输出调节输出、因此较轻负载输出上可能存在电压变化、我们捕获了辅助主机电源5V 电源输出上的观察结果。
谢谢
Sreenivasa