Other Parts Discussed in Thread: PMP9656
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:PMP9656 大家好、
您能帮我确认 PMP9656 的功率是否高达280W 吗?
280W (23.3A)是否可以共享效率曲线?
如果无法实现、则需要进行任何外部修改?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.