Other Parts Discussed in Thread: LM5060
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5060我想为电动自行车构建一个电池保护电路、该电路将电流限制在125A、但如果超过电流、该电路不会截止。电池电压为48V、使用太阳能充电。 我可以使用哪种限流器或 IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.