This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TINA/Spice:降压直流- DC原理图仿真相关问题

Guru**** 2560390 points
Other Parts Discussed in Thread: TINA-TI

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/716461/tina-spice-buck-dc-dc

主题中讨论的其他器件:TINA-TI

工具/软件:TINA-TI 或 Spice 模型

搭建了一个buck开环基本电路图(未加环路负反馈部分),输入激励3V直流电压,高侧 NMOS控制duty cycle为40 %,理论上输出

电压应该为3 *40%=1.2V。但是实际上仿真输出为3.28V。为什么?具体仿真波形细节请看附件。e2e.ti.com/.../4426.buck.TSC