Other Parts Discussed in Thread: CC1350STK, CC1350
主题: CC1350中讨论的其它部件
工具/软件:Linux
您好,
TI的CC1350 SensorTag是否兼容TI的15.4 堆栈Linux网关示例应用 ?
谢谢!
Patricio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC1350STK, CC1350
工具/软件:Linux
您好,
TI的CC1350 SensorTag是否兼容TI的15.4 堆栈Linux网关示例应用 ?
谢谢!
Patricio
Suyash Jain,
感谢您的回复。
我按照wiki的说明操作,尝试在TI资源管理器中实施COP示例:CC1350 LaunchPad->TI 802.15 .4 Stack->协处理器->TI-RTOS->CCS编译器->协处理器->应用程序->COP
但我发现了两个问题:
1)步骤(6)显示:"通过将第122行更改为:...,编辑Mac_user_config.h,它与Mac_user_config.c位于同一目录中。"
#if defined (CC1310EM_7xD_7793)7793)|| defined (CC1310EM_7ID)|| defined (module_CC13XX_7X7)
但第122行有一个"else (其他)"命令。
您是否介意用 "#if defined (CC13XX_LAUNCHXL)"的"99"行
2)步骤(8)说:..."将main.c的第369行编辑为"
#IF (CONFIG_RANGE_EXT_MODE == APIMAC_HIGH _GAIN_MODE)
但文件 main.c只有316行。
我做错了什么?
此致
Patricio