请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC1120 主题中讨论的其他部件:CC1200,
大家好,
在CC1120和CC1200的数据表中,我们都可以看到它们支持15.4g模式:
如我们所知,15.4g具有许多不同的RF配置组合(不同的速度,调制类型等),因此问题是CC1120/CC1200是否1200是否仅支持高于RF配置的配置,还是也可以配置为其他15.4g RF配置?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.