请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC1200 您好,
我们正在对其中一种设计进行原型设计,我们正在使用CC1200,并希望优化其速度,以便我们可以使用的默认SmartRF Studio设置发送12字节有效负载
169MHz载波,Symbol速率500kSPS,4-GFSK,最大吞吐量,ETSI标准
我们需要知道可以连续发送12字节有效负载的数据包的最快速度。 请提供帮助
-Pawan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.