请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC1352P7 我想知道 CC1352P1和 CC1352P7在868MHz频段中支持的最大数据速率。
两个组件的接收器滤波带宽均为4000KHZ (4MHz)。
P1支持2GFSK,P7支持4GFSK,SO
使用4GFSK的P7和 使用2GFSK的P1支持的最大数据速率是多少?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.