大家好、
我是一名学士学生、目前正在从事智能房间预订系统的工作。 应显示的数据将使用868MHz CC1101射频收发器发送。 不幸的是、我无法使数据传输可靠地工作。 我想我可以毫无问题地发送数据、通过将 IOCFG2设置为0x06、我可以在 GDO2上接收同步状态。 我还能够使用 SDR 和网络分析器查看数据。 但是、当我从 FIFO 读取数据时、即使 CRC 处于活动状态、它也是完全无用的。 我尝试寻找某种模式、但找不到任何东西。
我负责发送和接收 TI 提供的示例代码数据(如下论坛文章中所述: e2e.ti.com/.../cc1101-how-to-use-cc1101 )、但必须对其进行修改才能与我使用的控制器配合使用。 CC1101的配置使用针对灵敏度进行优化的默认76.8kBaud 配置文件直接从射频工作室导出。
我尝试过的 PCB 是一些中国 PCB、在这里我用 DigiKey 的原厂芯片、Mibot 的分线 PCB 以及使用 Johanson Tech 平衡-非平衡变压器和天线的定制 PCB 替换了芯片。 所有 PCB 都可以相互通信、但接收到的数据不会改变。
我要发送的数据与 TI 的示例代码中的数据几乎相同、我只添加了一些静态变量、以使接收到的数据更易读、并减小数据包大小。
是否有人知道我的问题可能是什么?
提前感谢。
printf("\n\n\n- = - = - = - = - = - = -\r\n");
printf("Register values acquired through the help of TI RFstudio\r\n");
CC1101_Init();
while (1)
{
// for(uint8_t counter = 0; counter < 0x2F; counter++)
// {
// printf("The register 0x%02X is set to: 0x%02X\r\n", counter, CC1101_SpiReadReg(counter));
// }
//Receiver code
if(!HAL_GPIO_ReadPin(btn0_GPIO_Port, btn0_Pin)) //If the button is not pressed on boot
{
printf("RX!\r\n\r\n"); //Show the user that RX mode has been selected and start the RX init
uint8_t rxBuffer[64] = {0}; //Init an empty rxBuffer for the received data
uint8_t rxBytes; //Init a variable with the amount of bytes in the RX FIFO
uint8_t marcstate; //Init a variable with the current CC1101 state
CC1101_SpiCmdStrobe(CC1101_SRX); //Set the CC1101 into RX mode
while(1)
{
if(HAL_GPIO_ReadPin(rfGDO2_GPIO_Port, rfGDO2_Pin)) //If GDO2 is high, indicating that a packet has been received
{
while(HAL_GPIO_ReadPin(rfGDO2_GPIO_Port, rfGDO2_Pin)); //As long as the device is still receiving, wait
rxBytes = CC1101_SpiReadReg(CC1101_RXBYTES); //Read number of bytes in RX FIFO
if(rxBytes != 0) //Check that we have bytes in FIFO
{
if(rxBytes & 0x80) //Check for RX FIFO overflow (MSB of RXBYTES)
{
CC1101_SpiCmdStrobe(CC1101_SFRX); //Flush RX FIFO
}
else
{
CC1101_SpiReadBurstReg(CC1101_RXFIFO , rxBuffer, rxBytes); //Read n bytes from RXFIFO
//Check CRC OK (CRC_OK: bit7 in second status byte)
//This assumes status bytes are appended in RX_FIFO
//(PKTCTRL1.APPEND_STATUS = 1)
//If CRC is disabled the CRC_OK field will read 1
if(rxBuffer[rxBytes - 1] & 0x80)
{
printf("The received #%d packet is:\r\n", rxPacketCounter);
for(uint8_t i = 0; i < PKTLEN; i++)
{
printf("0x%02X\r\n", rxBuffer[i]);
}
printf("\r\n\r\n");
//Update packet counter
rxPacketCounter++;
}
}
}
//Set radio back in RX
CC1101_SpiCmdStrobe(CC1101_SRX);
}
}
}
//Transmitter code
if(HAL_GPIO_ReadPin(btn0_GPIO_Port, btn0_Pin)) //If the button is pressed on boot
{
printf("TX!\r\n\r\n"); //Show the user that RX mode has been selected and start the TX init
uint8_t txBuffer[PKTLEN + 1] = {0}; //Initialize packet buffer of size PKTLEN + 1
txBuffer[3] = 0xAA;
txBuffer[4] = 0x55;
txBuffer[5] = 0x00;
txBuffer[6] = 0xFF;
while(1)
{
if(HAL_GPIO_ReadPin(btn0_GPIO_Port, btn0_Pin)) //Wait for a button push
{
do
{
txPacketCounter++; //Update packet counter
// Create a random packet with PKTLEN + 2 byte packet
// counter + n x random bytes
txBuffer[0] = PKTLEN; //Length byte
txBuffer[1] = (uint8_t) (txPacketCounter >> 8); //MSB of packetCounter
txBuffer[2] = (uint8_t) txPacketCounter; //LSB of packetCounter
CC1101_SpiWriteBurstReg(CC1101_TXFIFO, txBuffer, sizeof(txBuffer)); //Write packet to TX FIFO
CC1101_SpiCmdStrobe(CC1101_STX); //Strobe TX to send packet
//Wait for pin low that packet has been sent.
//(Assumes the GPIO connected to the radioRxTxISR function is
//set to GPIOx_CFG = 0x06)
while(HAL_GPIO_ReadPin(rfGDO2_GPIO_Port, rfGDO2_Pin)); //While the GDO2 pin is still high, the CC1101 is still transmitting
}while(!HAL_GPIO_ReadPin(btn0_GPIO_Port, btn0_Pin)); //Keep sending while the button is not pressed again
}
HAL_Delay(500);
}
}
}
#include <cc1101_v2.h>
#include <main.h>
/****************************************************************/
#define WRITE_BURST 0x40 //write burst
#define READ_SINGLE 0x80 //read single
#define READ_BURST 0xC0 //read burst
#define BYTES_IN_RXFIFO 0x7F //byte number in RXfifo
/****************************************************************/
uint8_t PaTabel[8] = {0x50, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
extern SPI_HandleTypeDef hspi1;
SPI_HandleTypeDef *pCC1101_hspi = &hspi1;
/****************************************************************
*FUNCTION NAME:SpiTransfer
*FUNCTION :spi transfer
*INPUT :value: data to send
*OUTPUT :data to receive
****************************************************************/
uint8_t CC1101_SpiTransfer(uint8_t value)
{
uint8_t rxData = 0;
HAL_SPI_TransmitReceive(pCC1101_hspi, &value, &rxData, 1, HAL_MAX_DELAY);
return rxData;
}
/****************************************************************
*FUNCTION NAME:Reset
*FUNCTION :CC1101 reset //details refer datasheet of CC1101/CC1100//
*INPUT :none
*OUTPUT :none
****************************************************************/
void CC1101_Reset (void)
{
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
HAL_Delay(1);
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
HAL_Delay(1);
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
CC1101_SpiTransfer(CC1101_SRES);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
}
/****************************************************************
*FUNCTION NAME:Init
*FUNCTION :CC1101 initialization
*INPUT :none
*OUTPUT :none
****************************************************************/
void CC1101_Init()
{
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
HAL_GPIO_WritePin(rfCLK_GPIO_Port, rfCLK_Pin, 1);
HAL_GPIO_WritePin(rfMOSI_GPIO_Port, rfMOSI_Pin, 0);
CC1101_Reset(); //CC1101 reset
CC1101_RegConfigSettings(); //CC1101 register config
CC1101_SpiWriteBurstReg(CC1101_PATABLE,PaTabel,8); //CC1101 PATABLE config
}
/****************************************************************
*FUNCTION NAME:SpiWriteReg
*FUNCTION :CC1101 write data to register
*INPUT :addr: register address; value: register value
*OUTPUT :none
****************************************************************/
void CC1101_SpiWriteReg(uint8_t addr, uint8_t value)
{
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
CC1101_SpiTransfer(addr);
CC1101_SpiTransfer(value);
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
}
/****************************************************************
*FUNCTION NAME:SpiWriteBurstReg
*FUNCTION :CC1101 write burst data to register
*INPUT :addr: register address; buffer:register value array; num:number to write
*OUTPUT :none
****************************************************************/
void CC1101_SpiWriteBurstReg(uint8_t addr, uint8_t *buffer, uint8_t num)
{
uint8_t i, temp;
temp = addr | WRITE_BURST;
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
CC1101_SpiTransfer(temp);
for (i = 0; i < num; i++)
{
CC1101_SpiTransfer(buffer[i]);
}
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
}
/****************************************************************
*FUNCTION NAME:SpiStrobe
*FUNCTION :CC1101 Strobe
*INPUT :strobe: command; //refer define in CC1101.h//
*OUTPUT :none
****************************************************************/
uint8_t CC1101_SpiCmdStrobe(uint8_t cmd)
{
uint8_t rc;
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0); //Pull the CS line low to init SPI communication
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin)); //Wait for the chip to be ready
HAL_SPI_TransmitReceive(pCC1101_hspi, &cmd, &rc, 1, HAL_MAX_DELAY);
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
return(rc);
//Old code
// HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
// while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
// CC1101_SpiTransfer(strobe);
// HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
}
/****************************************************************
*FUNCTION NAME:SpiReadReg
*FUNCTION :CC1101 read data from register
*INPUT :addr: register address
*OUTPUT :register value
****************************************************************/
uint8_t CC1101_SpiReadReg(uint8_t addr)
{
uint8_t temp, value;
temp = addr|READ_SINGLE;
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
CC1101_SpiTransfer(temp);
value = CC1101_SpiTransfer(0);
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
return value;
}
/****************************************************************
*FUNCTION NAME:SpiReadBurstReg
*FUNCTION :CC1101 read burst data from register
*INPUT :addr: register address; buffer:array to store register value; num: number to read
*OUTPUT :none
****************************************************************/
void CC1101_SpiReadBurstReg(uint8_t addr, uint8_t *buffer, uint8_t num)
{
uint8_t i,temp;
temp = addr | READ_BURST;
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
CC1101_SpiTransfer(temp);
for(i=0;i<num;i++)
{
buffer[i] = CC1101_SpiTransfer(0);
}
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
}
/****************************************************************
*FUNCTION NAME:SpiReadStatus
*FUNCTION :CC1101 read status register
*INPUT :addr: register address
*OUTPUT :status value
****************************************************************/
uint8_t CC1101_SpiReadStatus(uint8_t addr)
{
uint8_t value,temp;
temp = addr | READ_BURST;
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 0);
while(HAL_GPIO_ReadPin(rfMISO_GPIO_Port, rfMISO_Pin));
CC1101_SpiTransfer(temp);
value = CC1101_SpiTransfer(0);
HAL_GPIO_WritePin(rfCS_GPIO_Port, rfCS_Pin, 1);
return value;
}
/****************************************************************
*FUNCTION NAME:RegConfigSettings
*FUNCTION :CC1101 register config //details refer datasheet of CC1101/CC1100//
*INPUT :none
*OUTPUT :none
****************************************************************/
void CC1101_RegConfigSettings(void)
{
/* The following config has been retrieved from RF studio:
* - - - RF Parameters - - -
* Base Frequency: 867,999MHz
* Xtal Frequency 26MHz
* Modulation Format: GFSK
* Whitening: OFF (Default)
* Channel Number: 0 (Default)
* Data Rate: 1,19948kBaud
* Deviation: 5,157 471kHzs (Default)
* Channel Spacing: 199,951 172kHz (Default)
* RX Filter BW: 58,035 714kHz (Default)
* TX Power: 0dBm
* Manchester encoding disabled
* PA Ramping disabled
*
* - - - Packet TX settings: - - -
* Packet Data Size: 20, Add Seq. Number
* Packet Count: Infinite
* Text: "This is some data!"
* Advanced: on
* Sync Word Length: 30/32 sync word bits detected (Default)
* Preamble Count: 4, address field left empty
* Length config: Variable packet length mode. Paket length configured by the first byte after sync word
* Packet Interval: Use default
*/
reset();
CC1101_SpiWriteReg(CC1101_IOCFG2, 0x06);
CC1101_SpiWriteReg(CC1101_IOCFG1, 0x2E);
CC1101_SpiWriteReg(CC1101_IOCFG0, 0x06);
CC1101_SpiWriteReg(CC1101_FIFOTHR, 0x47);
CC1101_SpiWriteReg(CC1101_SYNC1, 0xD3);
CC1101_SpiWriteReg(CC1101_SYNC0, 0x91);
CC1101_SpiWriteReg(CC1101_PKTLEN, 0xFF);
CC1101_SpiWriteReg(CC1101_PKTCTRL1, 0x04);
CC1101_SpiWriteReg(CC1101_PKTCTRL0, 0x05);
CC1101_SpiWriteReg(CC1101_ADDR, 0x00);
CC1101_SpiWriteReg(CC1101_CHANNR, 0x00);
CC1101_SpiWriteReg(CC1101_FSCTRL1, 0x08);
CC1101_SpiWriteReg(CC1101_FSCTRL0, 0x00);
CC1101_SpiWriteReg(CC1101_FREQ2, 0x21);
CC1101_SpiWriteReg(CC1101_FREQ1, 0x62);
CC1101_SpiWriteReg(CC1101_FREQ0, 0x76);
CC1101_SpiWriteReg(CC1101_MDMCFG4, 0x7B);
CC1101_SpiWriteReg(CC1101_MDMCFG3, 0x83);
CC1101_SpiWriteReg(CC1101_MDMCFG2, 0x13);
CC1101_SpiWriteReg(CC1101_MDMCFG1, 0x22);
CC1101_SpiWriteReg(CC1101_MDMCFG0, 0xF8);
CC1101_SpiWriteReg(CC1101_DEVIATN, 0x42);
CC1101_SpiWriteReg(CC1101_MCSM2, 0x07);
CC1101_SpiWriteReg(CC1101_MCSM1, 0x30);
CC1101_SpiWriteReg(CC1101_MCSM0, 0x18);
CC1101_SpiWriteReg(CC1101_FOCCFG, 0x1D);
CC1101_SpiWriteReg(CC1101_BSCFG, 0x1C);
CC1101_SpiWriteReg(CC1101_AGCCTRL2, 0xC7);
CC1101_SpiWriteReg(CC1101_AGCCTRL1, 0x00);
CC1101_SpiWriteReg(CC1101_AGCCTRL0, 0xB2);
CC1101_SpiWriteReg(CC1101_WOREVT1, 0x87);
CC1101_SpiWriteReg(CC1101_WOREVT0, 0x6B);
CC1101_SpiWriteReg(CC1101_WORCTRL, 0xFB);
CC1101_SpiWriteReg(CC1101_FREND1, 0xB6);
CC1101_SpiWriteReg(CC1101_FREND0, 0x10);
CC1101_SpiWriteReg(CC1101_FSCAL3, 0xEA);
CC1101_SpiWriteReg(CC1101_FSCAL2, 0x2A);
CC1101_SpiWriteReg(CC1101_FSCAL1, 0x00);
CC1101_SpiWriteReg(CC1101_FSCAL0, 0x1F);
CC1101_SpiWriteReg(CC1101_RCCTRL1, 0x41);
CC1101_SpiWriteReg(CC1101_RCCTRL0, 0x00);
CC1101_SpiWriteReg(CC1101_FSTEST, 0x59);
CC1101_SpiWriteReg(CC1101_PTEST, 0x7F);
CC1101_SpiWriteReg(CC1101_AGCTEST, 0x3F);
CC1101_SpiWriteReg(CC1101_TEST2, 0x81);
CC1101_SpiWriteReg(CC1101_TEST1, 0x35);
CC1101_SpiWriteReg(CC1101_TEST0, 0x09);
//RF Studio Parameter Summary
/* Address Config = No address check */
/* Base Frequency = 867.999939 */
/* CRC Autoflush = false */
/* CRC Enable = true */
/* Carrier Frequency = 867.999939 */
/* Channel Number = 0 */
/* Channel Spacing = 199.951172 */
/* Data Format = Normal mode */
/* Data Rate = 1.19948 */
/* Deviation = 5.157471 */
/* Device Address = 0 */
/* Manchester Enable = false */
/* Modulated = true */
/* Modulation Format = GFSK */
/* PA Ramping = false */
/* Packet Length = 255 */
/* Packet Length Mode = Variable packet length mode. Packet length configured by the first byte after sync word */
/* Preamble Count = 4 */
/* RX Filter BW = 58.035714 */
/* Sync Word Qualifier Mode = 30/32 sync word bits detected */
/* TX Power = 0 */
/* Whitening = false */
}
/****************************************************************
*FUNCTION NAME:SendData
*FUNCTION :use CC1101 send data
*INPUT :txBuffer: data array to send; size: number of data to send, no more than 61
*OUTPUT :none
****************************************************************/
void CC1101_SendData(uint8_t *txBuffer,uint8_t size)
{
CC1101_SpiWriteReg(CC1101_TXFIFO,size);
CC1101_SpiWriteBurstReg(CC1101_TXFIFO,txBuffer,size); //write data to send
CC1101_SpiCmdStrobe(CC1101_STX); //start send
HAL_Delay(25);
CC1101_SpiCmdStrobe(CC1101_SFTX); //flush TXfifo
}
/****************************************************************
*FUNCTION NAME:SetReceive
*FUNCTION :set CC1101 to receive state
*INPUT :none
*OUTPUT :none
****************************************************************/
void CC1101_SetReceive(void)
{
CC1101_SpiCmdStrobe(CC1101_SRX);
}
/****************************************************************
*FUNCTION NAME:ReceiveData
*FUNCTION :read data received from RXfifo
*INPUT :rxBuffer: buffer to store data
*OUTPUT :size of data received
****************************************************************/
uint8_t CC1101_ReceiveData(uint8_t *rxBuffer)
{
uint8_t status[2];
uint8_t packetLength;
uint8_t length;
CC1101_SpiCmdStrobe(CC1101_SRX);
// This status register is safe to read since it will not be updated after
// the packet has been received
if((CC1101_SpiReadStatus(CC1101_RXBYTES) & BYTES_IN_RXFIFO))
{
// Read length byte
packetLength = CC1101_SpiReadReg(CC1101_RXFIFO);
// Read data from RX FIFO and store in rxBuffer
CC1101_SpiReadBurstReg(CC1101_RXFIFO, rxBuffer, packetLength);
length = packetLength;
// Read the 2 appended status bytes (status[0] = RSSI, status[1] = LQI)
CC1101_SpiReadBurstReg(CC1101_RXFIFO, status, 2);
//return the lenght of the packet
return length;
}
else
return 0;
}
// CC1101 CONFIG REGSITER #define CC1101_IOCFG2 0x00 // GDO2 output pin configuration #define CC1101_IOCFG1 0x01 // GDO1 output pin configuration #define CC1101_IOCFG0 0x02 // GDO0 output pin configuration #define CC1101_FIFOTHR 0x03 // RX FIFO and TX FIFO thresholds #define CC1101_SYNC1 0x04 // Sync word, high INT8U #define CC1101_SYNC0 0x05 // Sync word, low INT8U #define CC1101_PKTLEN 0x06 // Packet length #define CC1101_PKTCTRL1 0x07 // Packet automation control #define CC1101_PKTCTRL0 0x08 // Packet automation control #define CC1101_ADDR 0x09 // Device address #define CC1101_CHANNR 0x0A // Channel number #define CC1101_FSCTRL1 0x0B // Frequency synthesizer control #define CC1101_FSCTRL0 0x0C // Frequency synthesizer control #define CC1101_FREQ2 0x0D // Frequency control word, high INT8U #define CC1101_FREQ1 0x0E // Frequency control word, middle INT8U #define CC1101_FREQ0 0x0F // Frequency control word, low INT8U #define CC1101_MDMCFG4 0x10 // Modem configuration #define CC1101_MDMCFG3 0x11 // Modem configuration #define CC1101_MDMCFG2 0x12 // Modem configuration #define CC1101_MDMCFG1 0x13 // Modem configuration #define CC1101_MDMCFG0 0x14 // Modem configuration #define CC1101_DEVIATN 0x15 // Modem deviation setting #define CC1101_MCSM2 0x16 // Main Radio Control State Machine configuration #define CC1101_MCSM1 0x17 // Main Radio Control State Machine configuration #define CC1101_MCSM0 0x18 // Main Radio Control State Machine configuration #define CC1101_FOCCFG 0x19 // Frequency Offset Compensation configuration #define CC1101_BSCFG 0x1A // Bit Synchronization configuration #define CC1101_AGCCTRL2 0x1B // AGC control #define CC1101_AGCCTRL1 0x1C // AGC control #define CC1101_AGCCTRL0 0x1D // AGC control #define CC1101_WOREVT1 0x1E // High INT8U Event 0 timeout #define CC1101_WOREVT0 0x1F // Low INT8U Event 0 timeout #define CC1101_WORCTRL 0x20 // Wake On Radio control #define CC1101_FREND1 0x21 // Front end RX configuration #define CC1101_FREND0 0x22 // Front end TX configuration #define CC1101_FSCAL3 0x23 // Frequency synthesizer calibration #define CC1101_FSCAL2 0x24 // Frequency synthesizer calibration #define CC1101_FSCAL1 0x25 // Frequency synthesizer calibration #define CC1101_FSCAL0 0x26 // Frequency synthesizer calibration #define CC1101_RCCTRL1 0x27 // RC oscillator configuration #define CC1101_RCCTRL0 0x28 // RC oscillator configuration #define CC1101_FSTEST 0x29 // Frequency synthesizer calibration control #define CC1101_PTEST 0x2A // Production test #define CC1101_AGCTEST 0x2B // AGC test #define CC1101_TEST2 0x2C // Various test settings #define CC1101_TEST1 0x2D // Various test settings #define CC1101_TEST0 0x2E // Various test settings //CC1101 Strobe commands #define CC1101_SRES 0x30 // Reset chip. #define CC1101_SFSTXON 0x31 // Enable and calibrate frequency synthesizer (if MCSM0.FS_AUTOCAL=1). // If in RX/TX: Go to a wait state where only the synthesizer is // running (for quick RX / TX turnaround). #define CC1101_SXOFF 0x32 // Turn off crystal oscillator. #define CC1101_SCAL 0x33 // Calibrate frequency synthesizer and turn it off // (enables quick start). #define CC1101_SRX 0x34 // Enable RX. Perform calibration first if coming from IDLE and // MCSM0.FS_AUTOCAL=1. #define CC1101_STX 0x35 // In IDLE state: Enable TX. Perform calibration first if // MCSM0.FS_AUTOCAL=1. If in RX state and CCA is enabled: // Only go to TX if channel is clear. #define CC1101_SIDLE 0x36 // Exit RX / TX, turn off frequency synthesizer and exit // Wake-On-Radio mode if applicable. #define CC1101_SAFC 0x37 // Perform AFC adjustment of the frequency synthesizer #define CC1101_SWOR 0x38 // Start automatic RX polling sequence (Wake-on-Radio) #define CC1101_SPWD 0x39 // Enter power down mode when CSn goes high. #define CC1101_SFRX 0x3A // Flush the RX FIFO buffer. #define CC1101_SFTX 0x3B // Flush the TX FIFO buffer. #define CC1101_SWORRST 0x3C // Reset real time clock. #define CC1101_SNOP 0x3D // No operation. May be used to pad strobe commands to two // INT8Us for simpler software. //CC1101 STATUS REGSITER #define CC1101_PARTNUM 0x30 #define CC1101_VERSION 0x31 #define CC1101_FREQEST 0x32 #define CC1101_LQI 0x33 #define CC1101_RSSI 0x34 #define CC1101_MARCSTATE 0x35 #define CC1101_WORTIME1 0x36 #define CC1101_WORTIME0 0x37 #define CC1101_PKTSTATUS 0x38 #define CC1101_VCO_VC_DAC 0x39 #define CC1101_TXBYTES 0x3A #define CC1101_RXBYTES 0x3B //CC1101 PATABLE,TXFIFO,RXFIFO #define CC1101_PATABLE 0x3E #define CC1101_TXFIFO 0x3F #define CC1101_RXFIFO 0x3F void CC1101_SpiMode(void); uint8_t CC1101_SpiTransfer(uint8_t); void CC1101_Reset (void); void CC1101_SpiWriteReg(uint8_t, uint8_t); void CC1101_SpiWriteBurstReg(uint8_t, uint8_t*, uint8_t); uint8_t CC1101_SpiCmdStrobe(uint8_t); uint8_t CC1101_SpiReadReg(uint8_t); void CC1101_SpiReadBurstReg(uint8_t, uint8_t*, uint8_t); uint8_t CC1101_SpiReadStatus(uint8_t); void CC1101_RegConfigSettings(void); void CC1101_Init(void); void CC1101_SendData(uint8_t*, uint8_t); void CC1101_SetReceive(void); uint8_t CC1101_ReceiveData(uint8_t*);