This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/CC1125:CC1125寄存器

Guru**** 2535750 points
Other Parts Discussed in Thread: CC1125

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/808474/ccs-cc1125-cc1125-registers

器件型号:CC1125

工具/软件:Code Composer Studio

CC1125内置 CORDIC 内核、可以实时获取信号振幅和相位的采样值、但用户手册对相关寄存器的描述太简单了、所以对使用这些寄存器有一些疑问。

问题:寄存器0x2F84 (CORDIC [9:8]后的 ang1信号角)和0x2F85 (CORDIC [7:0]后的 Ang0信号角)存储一个10位相位采样值。 采样值是有符号数还是无符号数? 如果它是有符号数、它是否以二进制补码的形式表示?2。 对应于采样值0°~360°或其他角度范围的角度范围是多少?