请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC1200 我直接使用169MHz 建议电路、更改了数字寄存器频率值、发现其灵敏度相对于169MHz 下降了3db。
不建议直接在137MHz 至-158.3MHz 之间发送169MHz 电路。
原始工厂能否为我提供精确的137MHz--158.3MHz 推荐电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我直接使用169MHz 建议电路、更改了数字寄存器频率值、发现其灵敏度相对于169MHz 下降了3db。
不建议直接在137MHz 至-158.3MHz 之间发送169MHz 电路。
原始工厂能否为我提供精确的137MHz--158.3MHz 推荐电路?