This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P:在 rfWsnNodeExtFlashOadClient 示例中将 GPRAM 用作 RAM

Guru**** 2872500 points

Other Parts Discussed in Thread: CC1352P, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1175200/cc1352p-using-gpram-as-ram-in-rfwsnnodeextflashoadclient-example

器件型号:CC1352P
Thread 中讨论的其他器件: SysConfig

您好!  

我尝试在 rfWsnNodeExtFlashOadClient_CC1352P_4_LAUNCHXL_tirtos7_ticlang 示例中将 GPRAM 用作 RAM。

我尝试遵循 SDK 用户指南中有关如何执行该操作的说明、但在 OAD 片外示例中、我没有 CCFG 文件、因为 BIM 项目具有该文件。

这是我的 CMD 文件:

/******************************************************************************

 @file CC13X2_CC26X2_TIRTOS7_OAD.cmd

 @brief Over the Air Download Linker Command File

 Group: CMCU LPRF
 Target Device: cc13xx_cc26xx

 ******************************************************************************
 
 Copyright (c) 2017-2022, Texas Instruments Incorporated
 All rights reserved.

 Redistribution and use in source and binary forms, with or without
 modification, are permitted provided that the following conditions
 are met:

 *  Redistributions of source code must retain the above copyright
    notice, this list of conditions and the following disclaimer.

 *  Redistributions in binary form must reproduce the above copyright
    notice, this list of conditions and the following disclaimer in the
    documentation and/or other materials provided with the distribution.

 *  Neither the name of Texas Instruments Incorporated nor the names of
    its contributors may be used to endorse or promote products derived
    from this software without specific prior written permission.

 THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

 ******************************************************************************
 
 
 *****************************************************************************/


--stack_size=5192   /* C stack is also used for ISR stack */

HEAPSIZE = 0x4000;  /* Size of heap buffer used by HeapMem */

/* Retain interrupt vector table variable                                    */
--retain=g_pfnVectors
/* Override default entry point.                                             */
--entry_point ResetISR
/* Allow main() to take args                                                 */
--args 0x8
/* Suppress warnings and errors:                                             */
/* - 10063: Warning about entry point not being _c_int00                     */
/* - 16011, 16012: 8-byte alignment errors. Observed when linking in object  */
/*   files compiled using Keil (ARM compiler)                                */
--diag_suppress=10063,16011,16012

/* The following command line options are set as part of the CCS project.    */
/* If you are building using the command line, or for some reason want to    */
/* define them here, you can uncomment and modify these lines as needed.     */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone.              */
/*                                                                           */
/* --heap_size=0                                                             */
/* --stack_size=256                                                          */
/* --library=rtsv7M3_T_le_eabi.lib                                           */

/* The starting address of the application.  Normally the interrupt vectors  */
/* must be located at the beginning of the application.                      */

#ifdef OAD_ONCHIP
    #ifdef OAD_P_APP
        #define IMG_HDR                 0x44000
        #define FLASH_BASE              IMG_HDR + 0xA8
        #define FLASH_SIZE              0x56000 - FLASH_BASE
    #else
        #define IMG_HDR                 0x0
        #define FLASH_BASE              0xA8
        #define FLASH_SIZE              0x40000 - FLASH_BASE
    #endif
#else
    #define IMG_HDR                 0x0
    #define FLASH_BASE              0xA8
    #define FLASH_SIZE              0x56000 - FLASH_BASE
#endif

#define RAM_BASE                0x20000000
#define RAM_SIZE                0x14000
#define GPRAM_BASE              0x11000000
#define GPRAM_SIZE              0x2000

#define PAGE_SIZE               0x2000

/* System memory map */

MEMORY
{
    FLASH_IMG_HDR (RX) : origin = IMG_HDR, length = 0xA8

    /* Application stored in and executes from internal flash */
    FLASH (RX) : origin = FLASH_BASE, length = FLASH_SIZE
    /* Application uses internal RAM for data */
    SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
    /* Application can use GPRAM region as RAM if cache is disabled in the CCFG
    (DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
    GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
}

/* Section allocation in memory */

SECTIONS
{
    GROUP > FLASH_IMG_HDR
    {
        .image_header
    }

    .resetVecs      :   > FLASH_BASE LOAD_START(prgEntryAddr)
    .intvecs        :   > FLASH_BASE
    .text           :   >> FLASH
    .TI.ramfunc     : {} load=FLASH, run=SRAM, table(BINIT)
    .const          :   >> FLASH
    .constdata      :   >> FLASH
    .rodata         :   >> FLASH
    .binit          :   > FLASH
    .cinit          :   > FLASH  LOAD_END(flashEndAddr)
    .pinit          :   > FLASH
    .init_array     :   > FLASH
    .emb_text       :   >> FLASH
    //.ccfg           :   > FLASH (HIGH)

    .vtable         :   > SRAM
    .vtable_ram     :   > SRAM
     vtable_ram     :   > SRAM
    .data           :   > SRAM LOAD_START(ramStartHere)
    .bss            :   > SRAM
    .sysmem         :   > SRAM
    .stack          :   > SRAM (HIGH) LOAD_START(heapEnd)
    .nonretenvar    :   > SRAM
    /* Heap buffer used by HeapMem */
    .priheap   : {
        __primary_heap_start__ = .;
        . += HEAPSIZE;
        __primary_heap_end__ = .;
    } > SRAM align 8
    .gpram          :   > GPRAM
}

--symbol_map __TI_STACK_SIZE=__STACK_SIZE
--symbol_map __TI_STACK_BASE=__stack

-u_c_int00
--retain "*(.resetVecs)"
--retain "*(.vecs)"

SECTIONS
{
    .resetVecs: load > 0
    .vecs: load > 0x20000000, type = NOLOAD
}

当我单击"Device Configuration"时、我的 SysConfig 文件如下所示:

我在 cmd 文件中看到此注释,但我不确定应该将此定义放在哪里,我应该将其放在 BIM 项目中的 ccfg.c 文件中吗?

/* Application can use GPRAM region as RAM if cache is disabled in the CCFG
    (DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Michael、

    您将需要在 BIM 项目(CCFG 和链接器 cmd 文件)和应用项目(链接器 cmd 文件)中添加更改。

    谢谢、

    Mari H

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    不过、这是我的内存分配:

    因此它不起作用、因为它不使用 GPRAM 作为 RAM 来存储.bss 的一部分  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Michael、

    在您发布的链接器 cmd 文件中、.bss 仍设置为 SRAM。 (第142行)。

    谢谢、

    玛丽·H

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当我将.bss 设置到 GPRAM 时、它会给出以下错误:

    program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".bss" size 0x9c10. Available memory ranges: CC13X2_CC26X2_TIRTOS7_OAD.cmd 
    
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Michael、

    可以指示链接器将"尽可能多的.bss "放入 GPRAM 中。  

      .bss :
      {
        *(.bss)
      } > GPRAM

    谢谢、

    玛丽·H

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我如何说.bss 的再开采会进入 SRAM?

    这是 CMD 文件,它的静态工作:

    /******************************************************************************
    
     @file CC13X2_CC26X2_TIRTOS7_OAD.cmd
    
     @brief Over the Air Download Linker Command File
    
     Group: CMCU LPRF
     Target Device: cc13xx_cc26xx
    
     ******************************************************************************
     
     Copyright (c) 2017-2022, Texas Instruments Incorporated
     All rights reserved.
    
     Redistribution and use in source and binary forms, with or without
     modification, are permitted provided that the following conditions
     are met:
    
     *  Redistributions of source code must retain the above copyright
        notice, this list of conditions and the following disclaimer.
    
     *  Redistributions in binary form must reproduce the above copyright
        notice, this list of conditions and the following disclaimer in the
        documentation and/or other materials provided with the distribution.
    
     *  Neither the name of Texas Instruments Incorporated nor the names of
        its contributors may be used to endorse or promote products derived
        from this software without specific prior written permission.
    
     THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    
     ******************************************************************************
     
     
     *****************************************************************************/
    
    
    --stack_size=5192   /* C stack is also used for ISR stack */
    
    HEAPSIZE = 0x4000;  /* Size of heap buffer used by HeapMem */
    
    /* Retain interrupt vector table variable                                    */
    --retain=g_pfnVectors
    /* Override default entry point.                                             */
    --entry_point ResetISR
    /* Allow main() to take args                                                 */
    --args 0x8
    /* Suppress warnings and errors:                                             */
    /* - 10063: Warning about entry point not being _c_int00                     */
    /* - 16011, 16012: 8-byte alignment errors. Observed when linking in object  */
    /*   files compiled using Keil (ARM compiler)                                */
    --diag_suppress=10063,16011,16012
    
    /* The following command line options are set as part of the CCS project.    */
    /* If you are building using the command line, or for some reason want to    */
    /* define them here, you can uncomment and modify these lines as needed.     */
    /* If you are using CCS for building, it is probably better to make any such */
    /* modifications in your CCS project and leave this file alone.              */
    /*                                                                           */
    /* --heap_size=0                                                             */
    /* --stack_size=256                                                          */
    /* --library=rtsv7M3_T_le_eabi.lib                                           */
    
    /* The starting address of the application.  Normally the interrupt vectors  */
    /* must be located at the beginning of the application.                      */
    
    #ifdef OAD_ONCHIP
        #ifdef OAD_P_APP
            #define IMG_HDR                 0x44000
            #define FLASH_BASE              IMG_HDR + 0xA8
            #define FLASH_SIZE              0x56000 - FLASH_BASE
        #else
            #define IMG_HDR                 0x0
            #define FLASH_BASE              0xA8
            #define FLASH_SIZE              0x40000 - FLASH_BASE
        #endif
    #else
        #define IMG_HDR                 0x0
        #define FLASH_BASE              0xA8
        #define FLASH_SIZE              0x56000 - FLASH_BASE
    #endif
    
    #define RAM_BASE                0x20000000
    #define RAM_SIZE                0x14000
    #define GPRAM_BASE              0x11000000
    #define GPRAM_SIZE              0x2000
    
    #define PAGE_SIZE               0x2000
    
    /* System memory map */
    
    MEMORY
    {
        FLASH_IMG_HDR (RX) : origin = IMG_HDR, length = 0xA8
    
        /* Application stored in and executes from internal flash */
        FLASH (RX) : origin = FLASH_BASE, length = FLASH_SIZE
        /* Application uses internal RAM for data */
        SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
        /* Application can use GPRAM region as RAM if cache is disabled in the CCFG
        (DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
        GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
    }
    
    /* Section allocation in memory */
    
    SECTIONS
    {
        GROUP > FLASH_IMG_HDR
        {
            .image_header
        }
    
        .resetVecs      :   > FLASH_BASE LOAD_START(prgEntryAddr)
        .intvecs        :   > FLASH_BASE
        .text           :   >> FLASH
        .TI.ramfunc     : {} load=FLASH, run=SRAM, table(BINIT)
        .const          :   >> FLASH
        .constdata      :   >> FLASH
        .rodata         :   >> FLASH
        .binit          :   > FLASH
        .cinit          :   > FLASH  LOAD_END(flashEndAddr)
        .pinit          :   > FLASH
        .init_array     :   > FLASH
        .emb_text       :   >> FLASH
        //.ccfg           :   > FLASH (HIGH)
    
        .vtable         :   > SRAM
        .vtable_ram     :   > SRAM
         vtable_ram     :   > SRAM
        .data           :   > SRAM LOAD_START(ramStartHere)
        .bss            :   > SRAM
        .sysmem         :   > SRAM
        .stack          :   > SRAM (HIGH) LOAD_START(heapEnd)
        .nonretenvar    :   > SRAM
        /* Heap buffer used by HeapMem */
        .priheap   : {
            __primary_heap_start__ = .;
            . += HEAPSIZE;
            __primary_heap_end__ = .;
        } > SRAM align 8
        .gpram          :   > GPRAM
          .bss :
      {
        *(.bss)
      } > GPRAM
    }
    
    --symbol_map __TI_STACK_SIZE=__STACK_SIZE
    --symbol_map __TI_STACK_BASE=__stack
    
    -u_c_int00
    --retain "*(.resetVecs)"
    --retain "*(.vecs)"
    
    SECTIONS
    {
        .resetVecs: load > 0
        .vecs: load > 0x20000000, type = NOLOAD
    }
    

    错误信息:  

     line 153: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".bss" size 0x9c10.  Available memory ranges:
       GPRAM        size: 0x2000       unused: 0x2000       max hole: 0x2000 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我找到了我想要的正确语法:  

    .bss :
      {
        *(.bss)
      } >> GPRAM | SRAM
    }

    现在、分配如下所示:

    感谢您的帮助!