Other Parts Discussed in Thread: WMBUS
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC1125 主题中讨论的其他器件:WMBUS
符号速率与载波频率的关系、例如在智能射频 stdio 中、在200Kbps 范围内的最大频率为869MHz、而在169 MHz 范围内的最大频率仅为9.2kbps。
请澄清。
在169MHz 频率下也能实现200kbps。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.