This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] RTOS/CC1350:CC1350:使用频率(447mhz)?

Guru**** 2813875 points

Other Parts Discussed in Thread: CC1350

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/729755/rtos-cc1350-cc1350-use-frequency-447mhz

器件型号:CC1350

工具/软件:TI-RTOS

您好!

我对 CC1350有疑问。

#使用频率 问题。。

 CC1350数据表中注明了以下频段:

 1) 1.1特性1.
    全球首款双频带(低于1GHz 和2.4GHz)

 2) 1.2应用

   315、433、470、500、779、 868MHz、915MHz、 920MHz 和2.4GHz ISM 和 SRD 系统

=>那么、 如果看 2)、这是否不能使用447MHz 频带?

=>您能告诉我可以使用447MHz (SoC 或收发器)的其他产品吗?

谢谢主席先生-结束-