嗨、团队;
根据 TI 15.4中的收集器和传感器例程、我现在要通过传感器、每秒向收集器发送一个包含100个 ADC 数据的数据包。
不过、我发现在实际传输过程中、数据包传输时间远长于一秒、
因此、我想问一下是否有相应的解决方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
嗨、团队;
根据 TI 15.4中的收集器和传感器例程、我现在要通过传感器、每秒向收集器发送一个包含100个 ADC 数据的数据包。
不过、我发现在实际传输过程中、数据包传输时间远长于一秒、
因此、我想问一下是否有相应的解决方案。
在传感器部分、我将原来的发送温度数据部分替换为发送100个 ADC 数据。 从代码中可以看到、以下是从传感器到收集器发送数据部分的代码。 可以成功发送数据、但两次传输之间的时间间隔太长、无法完全满足工程要求。
static void processSensorMsgEvt(void)
{
Smsgs_sensorMsg_t sensor;
uint32_t stat;
memset(&sensor, 0, sizeof(Smsgs_sensorMsg_t));
ApiMac_mlmeGetReqUint32(ApiMac_attribute_diagRxSecureFail, &stat);
Sensor_msgStats.rxDecryptFailures = (uint16_t)stat;
ApiMac_mlmeGetReqUint32(ApiMac_attribute_diagTxSecureFail, &stat);
Sensor_msgStats.txEncryptFailures = (uint16_t)stat;
ApiMac_mlmeGetReqArray(ApiMac_attribute_extendedAddress,
sensor.extAddress);
/* fill in the message */
sensor.frameControl = configSettings.frameControl;
if(sensor.frameControl & Smsgs_dataFields_tempSensor)
{
memcpy(&sensor.tempSensor, &tempSensor,
sizeof(Smsgs_tempSensorField_t));
}
if(sensor.frameControl & Smsgs_dataFields_lightSensor)
{
memcpy(&sensor.lightSensor, &lightSensor,
sizeof(Smsgs_lightSensorField_t));
}
if(sensor.frameControl & Smsgs_dataFields_humiditySensor)
{
memcpy(&sensor.humiditySensor, &humiditySensor,
sizeof(Smsgs_humiditySensorField_t));
}
if(sensor.frameControl & Smsgs_dataFields_msgStats)
{
memcpy(&sensor.msgStats, &Sensor_msgStats,
sizeof(Smsgs_msgStatsField_t));
}
if(sensor.frameControl & Smsgs_dataFields_configSettings)
{
sensor.configSettings.pollingInterval = configSettings.pollingInterval;
sensor.configSettings.reportingInterval = configSettings
.reportingInterval;
}
/* inform the user interface */
Ssf_sensorReadingUpdate(&sensor);
/* send the data to the collector */
sendSensorMessage(&collectorAddr, &sensor);
}
static bool sendSensorMessage(ApiMac_sAddr_t *pDstAddr, Smsgs_sensorMsg_t *pMsg)
{
bool ret = false;
uint8_t *pMsgBuf;
uint16_t len = SMSGS_BASIC_SENSOR_LEN;
/* Figure out the length */
if(pMsg->frameControl & Smsgs_dataFields_tempSensor)
{
len += SMSGS_SENSOR_TEMP_LEN;
}
if(pMsg->frameControl & Smsgs_dataFields_lightSensor)
{
len += SMSGS_SENSOR_LIGHT_LEN;
}
if(pMsg->frameControl & Smsgs_dataFields_humiditySensor)
{
len += SMSGS_SENSOR_HUMIDITY_LEN;
}
if(pMsg->frameControl & Smsgs_dataFields_msgStats)
{
//len += SMSGS_SENSOR_MSG_STATS_LEN;
len += sizeof(Smsgs_msgStatsField_t);
}
if(pMsg->frameControl & Smsgs_dataFields_configSettings)
{
len += SMSGS_SENSOR_CONFIG_SETTINGS_LEN;
}
pMsgBuf = (uint8_t *)Ssf_malloc(len);
if(pMsgBuf)
{
uint8_t *pBuf = pMsgBuf;
*pBuf++ = (uint8_t)Smsgs_cmdIds_sensorData;
memcpy(pBuf, pMsg->extAddress, SMGS_SENSOR_EXTADDR_LEN);
pBuf += SMGS_SENSOR_EXTADDR_LEN;
pBuf = Util_bufferUint16(pBuf,pMsg->frameControl);
/* Buffer data in order of frameControl mask, starting with LSB */
if(pMsg->frameControl & Smsgs_dataFields_tempSensor)
{
for(int i=0;i<100;i++){
pBuf = Util_bufferUint16(pBuf, pMsg->tempSensor.ambienceTemp[i]);
}
//pBuf = Util_bufferUint16(pBuf, pMsg->tempSensor.ambienceTemp);
//pBuf = Util_bufferUint16(pBuf, pMsg->tempSensor.objectTemp);
}
if(pMsg->frameControl & Smsgs_dataFields_lightSensor)
{
pBuf = Util_bufferUint16(pBuf, pMsg->lightSensor.rawData);
}
if(pMsg->frameControl & Smsgs_dataFields_humiditySensor)
{
pBuf = Util_bufferUint16(pBuf, pMsg->humiditySensor.temp);
pBuf = Util_bufferUint16(pBuf, pMsg->humiditySensor.humidity);
}
if(pMsg->frameControl & Smsgs_dataFields_msgStats)
{
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.joinAttempts);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.joinFails);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.msgsAttempted);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.msgsSent);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.trackingRequests);
pBuf = Util_bufferUint16(pBuf,
pMsg->msgStats.trackingResponseAttempts);
pBuf = Util_bufferUint16(pBuf,
pMsg->msgStats.trackingResponseSent);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.configRequests);
pBuf = Util_bufferUint16(pBuf,
pMsg->msgStats.configResponseAttempts);
pBuf = Util_bufferUint16(pBuf,
pMsg->msgStats.configResponseSent);
pBuf = Util_bufferUint16(pBuf,
pMsg->msgStats.channelAccessFailures);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.macAckFailures);
pBuf = Util_bufferUint16(pBuf,
pMsg->msgStats.otherDataRequestFailures);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.syncLossIndications);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.rxDecryptFailures);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.txEncryptFailures);
pBuf = Util_bufferUint16(pBuf, Ssf_resetCount);
pBuf = Util_bufferUint16(pBuf, Ssf_resetReseason);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.joinTime);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.interimDelay);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.numBroadcastMsgRcvd);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.numBroadcastMsglost);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.avgE2EDelay);
pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.worstCaseE2EDelay);
}
if(pMsg->frameControl & Smsgs_dataFields_configSettings)
{
pBuf = Util_bufferUint32(pBuf,
pMsg->configSettings.reportingInterval);
pBuf = Util_bufferUint32(pBuf,
pMsg->configSettings.pollingInterval);
}
ret = Sensor_sendMsg(Smsgs_cmdIds_sensorData, pDstAddr, true, len, pMsgBuf);
if(ret == true){
LCD_WRITE_STRING("Data Success Send", 2);
}
else{
LCD_WRITE_STRING("Data Success Failed", 2);
}
Ssf_free(pMsgBuf);
}
return (ret);
}
Smsgs_tempSensorField_t修改后的结构
typedef struct _Smsgs_tempsensorfield_t
{
/*!
Ambience Chip Temperature - each value represents a 0.01 C
degree, so a value of 2475 represents 24.75 C.
*/
uint16_t ambienceTemp[100];
/*!
Object Temperature - each value represents a 0.01 C
degree, so a value of 2475 represents 24.75 C.
*/
//int16_t objectTemp;
} Smsgs_tempSensorField_t;是的,我调节发送消息的时间间隔,以每秒发送一次数据消息。 具体代码如下:
/////the part of sensor Configuration of time /*! Default Polling interval in milliseconds. It will get updated upon reception of a config request message */ #define CONFIG_POLLING_INTERVAL 6000 /*! PAN Advertisement Solicit trickle timer duration in milliseconds */ #define CONFIG_PAN_ADVERT_SOLICIT_CLK_DURATION 6000 /*! PAN Config Solicit trickle timer duration in milliseconds */ #define CONFIG_PAN_CONFIG_SOLICIT_CLK_DURATION 6000 /*! Default Reporting Interval - in milliseconds. It will get updated upon reception of a config request message */ #define CONFIG_REPORTING_INTERVAL 1000 #else /*! Default Polling interval in milliseconds. It will get updated upon reception of a config request message */ #define CONFIG_POLLING_INTERVAL 60000 /*! PAN Advertisement Solicit trickle timer duration in milliseconds */ #define CONFIG_PAN_ADVERT_SOLICIT_CLK_DURATION 60000 /*! PAN Config Solicit trickle timer duration in milliseconds */ #define CONFIG_PAN_CONFIG_SOLICIT_CLK_DURATION 60000 /*! Default Reporting Interval - in milliseconds. It will get updated upon reception of a config request message */ #define CONFIG_REPORTING_INTERVAL 600000 //////the part of collector Configuration of time /*! Reporting Interval - in milliseconds to be set on connected devices using configuration request messages */ #define CONFIG_REPORTING_INTERVAL 90000 /*! Polling interval in milliseconds to be set on connected devices using configuration request messages. Must be greater than or equal to default polling interval set on sensor devices */ #define CONFIG_POLLING_INTERVAL 6000 /*! Time interval in ms between tracking message intervals */ #define TRACKING_DELAY_TIME 60000 #else /*! Reporting Interval - in milliseconds to be set on connected devices using configuration request messages */ #define CONFIG_REPORTING_INTERVAL 1000 /*! Polling interval in milliseconds to be set on connected devices using configuration request messages. Must be greater than or equal to default polling interval set on sensor devices */ #define CONFIG_POLLING_INTERVAL 60000 /*! Time interval in ms between tracking message intervals */ #define TRACKING_DELAY_TIME 300000
通过以下函数'csf_deviceSensorDataUpdate (&pDataInd->srcAddr、pDataInd->RSSI、
sensorData);"" 打印数据。
"我发现在两块开发板上编写程序时、首次上电时、可以通过串行端口每秒打印一次 ADC 数据
但是、在"Configrap:0x1"出现后、两个开发板之间的数据包传输通常变得相对简单

尊敬的 Alex:
我尝试了以下方法。 在默认收集器、传感器项目中、我只将收集器和传感器中的报告间隔更改为1000。
这会导致传感器每秒报告一次。 这可以通过绿色 LED 切换间隔来看出。
因此、请 检查 是否由于您的应用更改而出现了延迟。
我建议您首先使用默认应用程序、使报告间隔为1000ms。 然后添加 ADC 数据变化。
如果由于函数中添加的 for 循环而确实出现了延迟,则可能应该将数据缓冲到该函数之外,并在进程中简单地传输 SensorMsgEvt()
此致、
SID