请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC1101 主题中讨论的其他器件: 测试2
我尝试使用 CC1101发送固定长度(40字节)的数据包。
我有以下代码用于测试,这是唯一正在 esp32上运行的任务:
void senderTask(void *arg){
static const char *TAG = "TX_TASK";
ESP_ERROR_CHECK(cc1101_init(CS_PIN, MISO_PIN,MOSI_PIN, SCLK_PIN, SPI_CLOCK, VSPI_HOST, GDO0_PIN));
int counter = 0;
while (true){
counter++;
// BEGIN TEST
ESP_LOGI(TAG, "msg: %u", counter);
// wait IDLE,
uint8_t reg_value = 0;
do {
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 00011111;
if (reg_value != 0x01){
cc1101_cmdStrobe(CC1101_SIDLE);
}
} while(reg_value != 0x01);
// define data to send
uint8_t data[40] = {39,0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88,0x99,0xaa,0xbb,0xcc,0xdd,0xee,0xff};
ESP_LOGI(TAG, "---------FIXED PACKET LENGTH---------");
// set fixed packet length mode
cc1101_writeReg(CC1101_PKTCTRL0,0x00);
// flush tx fifo
cc1101_cmdStrobe(CC1101_SFTX);
// write packet to fifo
cc1101_writeBurstReg(CC1101_TXFIFO, data,sizeof(data));
// check number of bytes written to the tx fifo
reg_value = cc1101_readStatusReg(CC1101_TXBYTES);
ESP_LOGI(TAG, "Number of bytes on tx fifo after burst write: %u", reg_value & 0b01111111);
// print status before tx
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
ESP_LOGI(TAG, "Status before tx: %u", reg_value);
// send TX strobe
cc1101_cmdStrobe(CC1101_STX);
// wait packet sended
vTaskDelay(100 / portTICK_PERIOD_MS);
// print status after tx
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
ESP_LOGI(TAG, "Status after tx: %u", reg_value);
// reset
cc1101_cmdStrobe(CC1101_SIDLE);
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
ESP_LOGI(TAG, "Status after resetting to idle: %u", reg_value);
ESP_LOGI(TAG, "---------VARIABLE PACKET LENGTH---------");
// set variable packet length mode
cc1101_writeReg(CC1101_PKTCTRL0,0x01);
// flush tx fifo
cc1101_cmdStrobe(CC1101_SFTX);
// write packet to fifo
cc1101_writeBurstReg(CC1101_TXFIFO, data,sizeof(data));
// check number of bytes written to the tx fifo
reg_value = cc1101_readStatusReg(CC1101_TXBYTES);
ESP_LOGI(TAG, "Number of bytes on tx fifo after burst write: %u", reg_value & 0b01111111);
// print status before tx
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
ESP_LOGI(TAG, "Status before tx: %u", reg_value);
// send TX strobe
cc1101_cmdStrobe(CC1101_STX);
// wait packet sended
vTaskDelay(100 / portTICK_PERIOD_MS);
// print status after tx
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
ESP_LOGI(TAG, "Status after tx: %u", reg_value);
// reset
cc1101_cmdStrobe(CC1101_SIDLE);
reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
ESP_LOGI(TAG, "Status after resetting to idle: %u", reg_value);
ESP_LOGI(TAG, "END LOOP\n\n");
// END TEST
// wait 1 second
vTaskDelay(1000 / portTICK_PERIOD_MS);
}
// hang foreveeee
while(true)vTaskDelay(100 / portTICK_PERIOD_MS);;
}
循环的一次迭代会输出以下内容:
I (220632) TX_TASK: msg: 180 I (220632) TX_TASK: ---------FIXED PACKET LENGTH--------- I (220642) TX_TASK: Number of bytes on tx fifo after burst write: 40 I (220642) TX_TASK: Status before tx: 1 I (220742) TX_TASK: Status after tx: 22 I (220742) TX_TASK: Status after resetting to idle: 1 I (220742) TX_TASK: ---------VARIABLE PACKET LENGTH--------- I (220752) TX_TASK: Number of bytes on tx fifo after burst write: 40 I (220762) TX_TASK: Status before tx: 1 I (220862) TX_TASK: Status after tx: 1 I (220862) TX_TASK: Status after resetting to idle: 1 I (220862) TX_TASK: END LOOP
您可以看到、对于相同的数据、使用固定的数据包长度会导致状态为22 (TX_undeflow)、而具有可变数据包的 CC1101会毫无问题地返回状态1 (IDLE)。 我不明白为什么会发生这种情况。 有人能解释我吗?
根据我从数据表中了解到的、在发送固定的数据包长度后、CC1101默认应该会返回到 IDLE 状态。
提前感谢您。
如果需要、可将用于初始化 CC1101的寄存器值如下所示:
/* Address Config = No address check */ /* Base Frequency = 433.919830 */ /* CRC Autoflush = false */ /* CRC Enable = false */ /* Carrier Frequency = 433.919830 */ /* Channel Number = 0 */ /* Channel Spacing = 199.951172 */ /* Data Format = Normal mode */ /* Data Rate = 0.0247955 */ /* Deviation = 47.607422 */ /* Device Address = 0 */ /* Manchester Enable = false */ /* Modulated = true */ /* Modulation Format = GFSK */ /* PA Ramping = false */ /* Packet Length = 40 */ /* Packet Length Mode = Variable packet length mode. Packet length configured by the first byte after sync word */ /* Preamble Count = 4 */ /* RX Filter BW = 58.035714 */ /* Sync Word Qualifier Mode = 16/16 sync word bits detected */ /* TX Power = 10 */ /* Whitening = false */ // RF settings for CC1101 // generated from smartRF 7 #define CC1101_DEFVAL_IOCFG2 0x29 // GDO2 Output Pin Configuration #define CC1101_DEFVAL_IOCFG1 0x2E // GDO1 Output Pin Configuration #define CC1101_DEFVAL_IOCFG0 0x06 // GDO0 Output Pin Configuration #define CC1101_DEFVAL_FIFOTHR 0x47 // RX FIFO and TX FIFO Thresholds #define CC1101_DEFVAL_SYNC1 0xD3 // Sync Word, High Byte #define CC1101_DEFVAL_SYNC0 0x91 // Sync Word, Low Byte #define CC1101_DEFVAL_PKTLEN 0x28 // Packet Length #define CC1101_DEFVAL_PKTCTRL1 0x00 // Packet Automation Control #define CC1101_DEFVAL_PKTCTRL0 0x01 // Packet Automation Control #define CC1101_DEFVAL_ADDR 0x00 // Device Address #define CC1101_DEFVAL_CHANNR 0x00 // Channel Number #define CC1101_DEFVAL_FSCTRL1 0x0F // Frequency Synthesizer Control #define CC1101_DEFVAL_FSCTRL0 0x00 // Frequency Synthesizer Control #define CC1101_DEFVAL_FREQ2 0x10 // Frequency Control Word, High Byte #define CC1101_DEFVAL_FREQ1 0xB0 // Frequency Control Word, Middle Byte #define CC1101_DEFVAL_FREQ0 0x71 // Frequency Control Word, Low Byte #define CC1101_DEFVAL_MDMCFG4 0xF0 // Modem Configuration #define CC1101_DEFVAL_MDMCFG3 0x00 // Modem Configuration #define CC1101_DEFVAL_MDMCFG2 0x12 // Modem Configuration #define CC1101_DEFVAL_MDMCFG1 0x22 // Modem Configuration #define CC1101_DEFVAL_MDMCFG0 0xF8 // Modem Configuration #define CC1101_DEFVAL_DEVIATN 0x47 // Modem Deviation Setting #define CC1101_DEFVAL_MCSM2 0x07 // Main Radio Control State Machine Configuration #define CC1101_DEFVAL_MCSM1 0x30 // Main Radio Control State Machine Configuration #define CC1101_DEFVAL_MCSM0 0x04 // Main Radio Control State Machine Configuration #define CC1101_DEFVAL_FOCCFG 0x36 // Frequency Offset Compensation Configuration #define CC1101_DEFVAL_BSCFG 0x6C // Bit Synchronization Configuration #define CC1101_DEFVAL_AGCCTRL2 0x03 // AGC Control #define CC1101_DEFVAL_AGCCTRL1 0x40 // AGC Control #define CC1101_DEFVAL_AGCCTRL0 0x91 // AGC Control #define CC1101_DEFVAL_WOREVT1 0x87 // High Byte Event0 Timeout #define CC1101_DEFVAL_WOREVT0 0x6B // Low Byte Event0 Timeout #define CC1101_DEFVAL_WORCTRL 0xF8 // Wake On Radio Control #define CC1101_DEFVAL_FREND1 0x56 // Front End RX Configuration #define CC1101_DEFVAL_FREND0 0x10 // Front End TX Configuration #define CC1101_DEFVAL_FSCAL3 0xE9 // Frequency Synthesizer Calibration #define CC1101_DEFVAL_FSCAL2 0x2A // Frequency Synthesizer Calibration #define CC1101_DEFVAL_FSCAL1 0x00 // Frequency Synthesizer Calibration #define CC1101_DEFVAL_FSCAL0 0x1F // Frequency Synthesizer Calibration #define CC1101_DEFVAL_RCCTRL1 0x41 // RC Oscillator Configuration #define CC1101_DEFVAL_RCCTRL0 0x00 // RC Oscillator Configuration #define CC1101_DEFVAL_FSTEST 0x59 // Frequency Synthesizer Calibration Control #define CC1101_DEFVAL_PTEST 0x7F // Production Test #define CC1101_DEFVAL_AGCTEST 0x3F // AGC Test #define CC1101_DEFVAL_TEST2 0x81 // Various Test Settings #define CC1101_DEFVAL_TEST1 0x35 // Various Test Settings #define CC1101_DEFVAL_TEST0 0x09 // Various Test Settings #define CC1101_DEFVAL_PARTNUM 0x00 // Chip ID #define CC1101_DEFVAL_VERSION 0x04 // Chip ID #define CC1101_DEFVAL_FREQEST 0x00 // Frequency Offset Estimate from Demodulator #define CC1101_DEFVAL_LQI 0x00 // Demodulator Estimate for Link Quality #define CC1101_DEFVAL_RSSI 0x00 // Received Signal Strength Indication #define CC1101_DEFVAL_MARCSTATE 0x00 // Main Radio Control State Machine State #define CC1101_DEFVAL_WORTIME1 0x00 // High Byte of WOR Time #define CC1101_DEFVAL_WORTIME0 0x00 // Low Byte of WOR Time #define CC1101_DEFVAL_PKTSTATUS 0x00 // Current GDOx Status and Packet Status #define CC1101_DEFVAL_VCO_VC_DAC 0x00 // Current Setting from PLL Calibration Module #define CC1101_DEFVAL_TXBYTES 0x00 // Underflow and Number of Bytes #define CC1101_DEFVAL_RXBYTES 0x00 // Overflow and Number of Bytes #define CC1101_DEFVAL_RCCTRL1_STATUS 0x00 // Last RC Oscillator Calibration Result #define CC1101_DEFVAL_RCCTRL0_STATUS 0x00 // Last RC Oscillator Calibration Result // change power output #define CC1101_DEFVAL_PATABLE 0xc0