This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1101:以固定数据包长度模式发送数据包会触发 fifo_underflow 状态

Guru**** 2611705 points
Other Parts Discussed in Thread: CC1101

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1327886/cc1101-sending-packets-on-fixed-packet-length-mode-triggers-state-fifo_underflow

器件型号:CC1101
主题中讨论的其他器件: 测试2

我尝试使用 CC1101发送固定长度(40字节)的数据包。

我有以下代码用于测试,这是唯一正在 esp32上运行的任务:

void senderTask(void *arg){
    static const char *TAG = "TX_TASK";

    ESP_ERROR_CHECK(cc1101_init(CS_PIN, MISO_PIN,MOSI_PIN, SCLK_PIN, SPI_CLOCK, VSPI_HOST, GDO0_PIN));

    int counter = 0;

    while (true){
        counter++;


        // BEGIN TEST
        ESP_LOGI(TAG, "msg: %u", counter);

            // wait IDLE,
        uint8_t reg_value = 0;
        do {
            reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 00011111;
            if (reg_value != 0x01){
                cc1101_cmdStrobe(CC1101_SIDLE);
            }
        } while(reg_value != 0x01);


        // define data to send
        uint8_t data[40] = {39,0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88,0x99,0xaa,0xbb,0xcc,0xdd,0xee,0xff};


        ESP_LOGI(TAG, "---------FIXED PACKET LENGTH---------");
        // set fixed packet length mode
        cc1101_writeReg(CC1101_PKTCTRL0,0x00);

        // flush tx fifo
        cc1101_cmdStrobe(CC1101_SFTX);

        // write packet to fifo
        cc1101_writeBurstReg(CC1101_TXFIFO, data,sizeof(data));

        // check number of bytes written to the tx fifo
        reg_value = cc1101_readStatusReg(CC1101_TXBYTES);
        ESP_LOGI(TAG, "Number of bytes on tx fifo after burst write: %u", reg_value & 0b01111111);


        // print status before tx
        reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
        ESP_LOGI(TAG, "Status before tx: %u", reg_value);

        // send TX strobe
        cc1101_cmdStrobe(CC1101_STX);

        // wait packet sended
        vTaskDelay(100 / portTICK_PERIOD_MS);

        // print status after tx
        reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
        ESP_LOGI(TAG, "Status after tx: %u", reg_value);


        // reset
        cc1101_cmdStrobe(CC1101_SIDLE);
        reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
        ESP_LOGI(TAG, "Status after resetting to idle: %u", reg_value);




        ESP_LOGI(TAG, "---------VARIABLE PACKET LENGTH---------");
        // set variable packet length mode
        cc1101_writeReg(CC1101_PKTCTRL0,0x01);


        // flush tx fifo
        cc1101_cmdStrobe(CC1101_SFTX);

        // write packet to fifo
        cc1101_writeBurstReg(CC1101_TXFIFO, data,sizeof(data));

        // check number of bytes written to the tx fifo
        reg_value = cc1101_readStatusReg(CC1101_TXBYTES);
        ESP_LOGI(TAG, "Number of bytes on tx fifo after burst write: %u", reg_value & 0b01111111);

        // print status before tx
        reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
        ESP_LOGI(TAG, "Status before tx: %u", reg_value);

        // send TX strobe
        cc1101_cmdStrobe(CC1101_STX);

        // wait packet sended
        vTaskDelay(100 / portTICK_PERIOD_MS);

        // print status after tx
        reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
        ESP_LOGI(TAG, "Status after tx: %u", reg_value);



        // reset
        cc1101_cmdStrobe(CC1101_SIDLE);
        reg_value = cc1101_readStatusReg(CC1101_MARCSTATE) & 0b00011111;
        ESP_LOGI(TAG, "Status after resetting to idle: %u", reg_value);
        ESP_LOGI(TAG, "END LOOP\n\n"); 

        // END TEST

        // wait 1 second
        vTaskDelay(1000 / portTICK_PERIOD_MS);
    }

    // hang foreveeee
    while(true)vTaskDelay(100 / portTICK_PERIOD_MS);;

}

循环的一次迭代会输出以下内容:

I (220632) TX_TASK: msg: 180
I (220632) TX_TASK: ---------FIXED PACKET LENGTH---------
I (220642) TX_TASK: Number of bytes on tx fifo after burst write: 40
I (220642) TX_TASK: Status before tx: 1
I (220742) TX_TASK: Status after tx: 22
I (220742) TX_TASK: Status after resetting to idle: 1
I (220742) TX_TASK: ---------VARIABLE PACKET LENGTH---------
I (220752) TX_TASK: Number of bytes on tx fifo after burst write: 40
I (220762) TX_TASK: Status before tx: 1
I (220862) TX_TASK: Status after tx: 1
I (220862) TX_TASK: Status after resetting to idle: 1
I (220862) TX_TASK: END LOOP

您可以看到、对于相同的数据、使用固定的数据包长度会导致状态为22 (TX_undeflow)、而具有可变数据包的 CC1101会毫无问题地返回状态1 (IDLE)。 我不明白为什么会发生这种情况。 有人能解释我吗?

根据我从数据表中了解到的、在发送固定的数据包长度后、CC1101默认应该会返回到 IDLE 状态。

提前感谢您。

如果需要、可将用于初始化 CC1101的寄存器值如下所示:

/* Address Config = No address check */
/* Base Frequency = 433.919830 */
/* CRC Autoflush = false */
/* CRC Enable = false */
/* Carrier Frequency = 433.919830 */
/* Channel Number = 0 */
/* Channel Spacing = 199.951172 */
/* Data Format = Normal mode */
/* Data Rate = 0.0247955 */
/* Deviation = 47.607422 */
/* Device Address = 0 */
/* Manchester Enable = false */
/* Modulated = true */
/* Modulation Format = GFSK */
/* PA Ramping = false */
/* Packet Length = 40 */
/* Packet Length Mode = Variable packet length mode. Packet length configured by the first byte after sync word */
/* Preamble Count = 4 */
/* RX Filter BW = 58.035714 */
/* Sync Word Qualifier Mode = 16/16 sync word bits detected */
/* TX Power = 10 */
/* Whitening = false */
// RF settings for CC1101
// generated from smartRF 7

#define CC1101_DEFVAL_IOCFG2            0x29    // GDO2 Output Pin Configuration
#define CC1101_DEFVAL_IOCFG1            0x2E    // GDO1 Output Pin Configuration
#define CC1101_DEFVAL_IOCFG0            0x06    // GDO0 Output Pin Configuration
#define CC1101_DEFVAL_FIFOTHR           0x47    // RX FIFO and TX FIFO Thresholds
#define CC1101_DEFVAL_SYNC1             0xD3    // Sync Word, High Byte
#define CC1101_DEFVAL_SYNC0             0x91    // Sync Word, Low Byte
#define CC1101_DEFVAL_PKTLEN            0x28    // Packet Length
#define CC1101_DEFVAL_PKTCTRL1          0x00    // Packet Automation Control
#define CC1101_DEFVAL_PKTCTRL0          0x01    // Packet Automation Control
#define CC1101_DEFVAL_ADDR              0x00    // Device Address
#define CC1101_DEFVAL_CHANNR            0x00    // Channel Number
#define CC1101_DEFVAL_FSCTRL1           0x0F    // Frequency Synthesizer Control
#define CC1101_DEFVAL_FSCTRL0           0x00    // Frequency Synthesizer Control
#define CC1101_DEFVAL_FREQ2             0x10    // Frequency Control Word, High Byte
#define CC1101_DEFVAL_FREQ1             0xB0    // Frequency Control Word, Middle Byte
#define CC1101_DEFVAL_FREQ0             0x71    // Frequency Control Word, Low Byte
#define CC1101_DEFVAL_MDMCFG4           0xF0    // Modem Configuration
#define CC1101_DEFVAL_MDMCFG3           0x00    // Modem Configuration
#define CC1101_DEFVAL_MDMCFG2           0x12    // Modem Configuration
#define CC1101_DEFVAL_MDMCFG1           0x22    // Modem Configuration
#define CC1101_DEFVAL_MDMCFG0           0xF8    // Modem Configuration
#define CC1101_DEFVAL_DEVIATN           0x47    // Modem Deviation Setting
#define CC1101_DEFVAL_MCSM2             0x07    // Main Radio Control State Machine Configuration
#define CC1101_DEFVAL_MCSM1             0x30    // Main Radio Control State Machine Configuration
#define CC1101_DEFVAL_MCSM0             0x04    // Main Radio Control State Machine Configuration
#define CC1101_DEFVAL_FOCCFG            0x36    // Frequency Offset Compensation Configuration
#define CC1101_DEFVAL_BSCFG             0x6C    // Bit Synchronization Configuration
#define CC1101_DEFVAL_AGCCTRL2          0x03    // AGC Control
#define CC1101_DEFVAL_AGCCTRL1          0x40    // AGC Control
#define CC1101_DEFVAL_AGCCTRL0          0x91    // AGC Control
#define CC1101_DEFVAL_WOREVT1           0x87    // High Byte Event0 Timeout
#define CC1101_DEFVAL_WOREVT0           0x6B    // Low Byte Event0 Timeout
#define CC1101_DEFVAL_WORCTRL           0xF8    // Wake On Radio Control
#define CC1101_DEFVAL_FREND1            0x56    // Front End RX Configuration
#define CC1101_DEFVAL_FREND0            0x10    // Front End TX Configuration
#define CC1101_DEFVAL_FSCAL3            0xE9    // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_FSCAL2            0x2A    // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_FSCAL1            0x00    // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_FSCAL0            0x1F    // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_RCCTRL1           0x41    // RC Oscillator Configuration
#define CC1101_DEFVAL_RCCTRL0           0x00    // RC Oscillator Configuration
#define CC1101_DEFVAL_FSTEST            0x59    // Frequency Synthesizer Calibration Control
#define CC1101_DEFVAL_PTEST             0x7F    // Production Test
#define CC1101_DEFVAL_AGCTEST           0x3F    // AGC Test
#define CC1101_DEFVAL_TEST2             0x81    // Various Test Settings
#define CC1101_DEFVAL_TEST1             0x35    // Various Test Settings
#define CC1101_DEFVAL_TEST0             0x09    // Various Test Settings
#define CC1101_DEFVAL_PARTNUM           0x00    // Chip ID
#define CC1101_DEFVAL_VERSION           0x04    // Chip ID
#define CC1101_DEFVAL_FREQEST           0x00    // Frequency Offset Estimate from Demodulator
#define CC1101_DEFVAL_LQI               0x00    // Demodulator Estimate for Link Quality
#define CC1101_DEFVAL_RSSI              0x00    // Received Signal Strength Indication
#define CC1101_DEFVAL_MARCSTATE         0x00    // Main Radio Control State Machine State
#define CC1101_DEFVAL_WORTIME1          0x00    // High Byte of WOR Time
#define CC1101_DEFVAL_WORTIME0          0x00    // Low Byte of WOR Time
#define CC1101_DEFVAL_PKTSTATUS         0x00    // Current GDOx Status and Packet Status
#define CC1101_DEFVAL_VCO_VC_DAC        0x00    // Current Setting from PLL Calibration Module
#define CC1101_DEFVAL_TXBYTES           0x00    // Underflow and Number of Bytes
#define CC1101_DEFVAL_RXBYTES           0x00    // Overflow and Number of Bytes
#define CC1101_DEFVAL_RCCTRL1_STATUS    0x00    // Last RC Oscillator Calibration Result
#define CC1101_DEFVAL_RCCTRL0_STATUS    0x00    // Last RC Oscillator Calibration Result



// change power output
#define CC1101_DEFVAL_PATABLE 0xc0

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好

    我无法重现您的问题:

    我测试了以下设置:

    static const registerSetting_t preferredSettings[]= 
    {
        {CC1101_IOCFG2, 0x29},
        {CC1101_IOCFG1, 0x2E},
        {CC1101_IOCFG0, 0x06},
        {CC1101_FIFOTHR, 0x47},
        {CC1101_SYNC1, 0xD3},
        {CC1101_SYNC0, 0x91},
        {CC1101_PKTLEN, 0x28},
        {CC1101_PKTCTRL1, 0x00},
        {CC1101_PKTCTRL0, 0x00},
        {CC1101_ADDR, 0x00},
        {CC1101_CHANNR, 0x00},
        {CC1101_FSCTRL1, 0x0F},
        {CC1101_FSCTRL0, 0x00},
        {CC1101_FREQ2, 0x10},
        {CC1101_FREQ1, 0xB0},
        {CC1101_FREQ0, 0x71},
        {CC1101_MDMCFG4, 0xF0},
        {CC1101_MDMCFG3, 0x00},
        {CC1101_MDMCFG2, 0x12},
        {CC1101_MDMCFG1, 0x22},
        {CC1101_MDMCFG0, 0xF8},
        {CC1101_DEVIATN, 0x47},
        {CC1101_MCSM2, 0x07},
        {CC1101_MCSM1, 0x30},
        {CC1101_MCSM0, 0x04},
        {CC1101_FOCCFG, 0x16},
        {CC1101_BSCFG, 0x6C},
        {CC1101_AGCCTRL2, 0x03},
        {CC1101_AGCCTRL1, 0x40},
        {CC1101_AGCCTRL0, 0x91},
        {CC1101_WOREVT1, 0x87},
        {CC1101_WOREVT0, 0x6B},
        {CC1101_WORCTRL, 0xFB},
        {CC1101_FREND1, 0x56},
        {CC1101_FREND0, 0x10},
        {CC1101_FSCAL3, 0xE9},
        {CC1101_FSCAL2, 0x2A},
        {CC1101_FSCAL1, 0x00},
        {CC1101_FSCAL0, 0x1F},
        {CC1101_RCCTRL1, 0x41},
        {CC1101_RCCTRL0, 0x00},
        {CC1101_FSTEST, 0x59},
        {CC1101_PTEST, 0x7F},
        {CC1101_AGCTEST, 0x3F},
        {CC1101_TEST2, 0x81},
        {CC1101_TEST1, 0x35},
        {CC1101_TEST0, 0x09},
    };

    void main(void) {
    
        // Initialize MCU and peripherals
        initMCU();
    
        // Write radio registers
        registerConfig();
        
        uint8 txBuffer[40] = {39,0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88,0x99,0xaa,0xbb,0xcc,0xdd,0xee,0xff};
    
        // Connect ISR function to GPIO2
        ioPinIntRegister(IO_PIN_PORT_1, GPIO0, &radioTxISR);
    
        // Interrupt on falling edge
        ioPinIntTypeSet(IO_PIN_PORT_1, GPIO0, IO_PIN_FALLING_EDGE);
    
        // Clear ISR flag
        ioPinIntClear(IO_PIN_PORT_1, GPIO0);
    
        // Enable interrupt
        ioPinIntEnable(IO_PIN_PORT_1, GPIO0);
    
        // Infinite loop
        while(TRUE) 
        {
            // Write packet to TX FIFO
            cc1101SpiWriteTxFifo(txBuffer,sizeof(txBuffer));
                    
            cc1101SpiReadReg(CC1101_TXBYTES, &temp, 1);   // temp = 0x28
            
            // Strobe TX to send packet
            trxSpiCmdStrobe(CC1101_STX);
    
            // Wait for interrupt that packet has been sent.
            // (Assumes the GPIO connected to the radioRxTxISR function is
            // set to GPIOx_CFG = 0x06)
            while(packetSemaphore != ISR_ACTION_REQUIRED);
                    
            cc1101SpiReadReg(CC1101_TXBYTES, &temp, 1);   // temp = 0
            cc1101SpiReadReg(CC1101_MARCSTATE, &temp, 1); // Temp = 0x01 (IDLE)
                    
            // Clear semaphore flag
            packetSemaphore = ISR_IDLE;
        }
    }

    我已经验证了使用调试器读取的温度值。

    唯一的区别是、我使用中断来实际确保数据包已发送(不应为此使用软件延迟)

    您的代码的其他问题是您没有按照我所能看到的方式校准合成器。

    此外、我不明白为什么在数据包仅为16字节时使用40这一固定长度。

    Siri

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的帮助、我终于找到了我的问题。 给我看看。"

    我忘记调用 setRegisters ()函数,这使 PKTLEN 设置为默认值255。 这就是可变数据包长度起作用但固定数据包长度不起作用的原因。 (因为它预期一个255字节的数据包)