Other Parts Discussed in Thread: TLV61047
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLV61047 工具/软件:
大家好!
我对 TLV61047有疑问。
是否有任何展示输出电压精度的文档?
例如、
它可以输出15V、误差为±3%。
我想知道110mA 当输入为5V±10%时 IOUT=IOUT=15V 时的输出误差。
此致、
Ishiwata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.