大家好,
我正在使用TMUX646进行I2C mutxing,这样我就可以使用2 mipi摄像机了。 我使用的是用于POC的IMX8MP自定义板,Linux在默认情况下没有TMUX646的驱动程序。
请帮助我们在我的主板中增加对TMUX646的支持,并建议我们如何向前推进
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我连接TMUX646的方式是:
TMUX646从IMX8MP处理器接收输入,从TMUX646输出,我连接了2个MIPI摄像头。
现在我了解的是处理器端的流量,我们可以使用TMUX646的SEL针来选择摄像机,但为了完成通信,我们需要有mipi摄像机和TMUX646的驱动器。 我在Imx8MP的Yocto SDK中已经有mipi相机的驱动程序,但没有TMUX646的驱动程序。
我只想得到你们的帮助,让大家找到TMUX646的驱动程序,否则我需要自己写整个驱动程序。
Linux确实有 一个驱动程序,即i2c-mix-gpio。