Other Parts Discussed in Thread: TMUX7219
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TMUX7219您好!
我正在寻找一款 SPDT 多路复用器、该多路复用器能够传输48V 信号并在不到300ns 的时间内切换。
基本上、我希望在不到300ns 的时间内在25V 和48V 的2个电源之间切换。
(如果需要、我有一个48V PS)。
此致、
Giora
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.