请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMUX6112 您好!
TMUX6112是否可与 Vdd=+7V 和 VSS=-4.5V 搭配使用?
VDD 至 VSS 的电压范围为10V 至34V。
VSS 到 GND 的电压范围是否应为-5V 至-17V?
谢谢、
Shimon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.