请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN74LVC1G66 你(们)好
我需要将1.2V POD12复位输出从其中一个控制器传递到存储器芯片(一旦控制器脱离复位状态)。
计划使用74LVC1G66、控制器的复位信号(1.8V 电平)控制引脚。
输入为1.2V POD12、输出应驱动 POD12 DDR 存储器芯片。
VCC 可以是3.3V/1.8V。
CAN 74LVC1G66适用于此应用。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
我需要将1.2V POD12复位输出从其中一个控制器传递到存储器芯片(一旦控制器脱离复位状态)。
计划使用74LVC1G66、控制器的复位信号(1.8V 电平)控制引脚。
输入为1.2V POD12、输出应驱动 POD12 DDR 存储器芯片。
VCC 可以是3.3V/1.8V。
CAN 74LVC1G66适用于此应用。