请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TS5A3160 您好!
通常、如果 VCC = 0V、则会将器件置于关断模式。 但是、如果 VCC 仍然连接到5V、但 GND 断开或保持开路、它是否也会进入关断模式?
谢谢。
- YY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.