Other Parts Discussed in Thread: TS5A2066, TMUX136
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TS5A2066 主题中讨论的其他器件: TMUX136
您好!
TS5A2066数据表显示、10MHz 时的关断隔离为-68dB。 1GHz 和10GHz 的数据是什么? 数据是否优于或差于10MHz?
谢谢!
-落基山脉
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.